Other topics about Sample Programs
This section explains how to control the E5061B by using WinSock API in the Windows environment.
Opening ctrl_lan.xls in Microsoft Excel displays the screen shown in the figure below.

For how to use each element in ctrl_lan.xls, refer to the following description.
Enter the version number of WinSock API in the cell to the right side of "Winsock Version." The version number is obtained by multiplying 256 by the major version and then adding the minor version. For example, when the version of your Winsock API is 1.1, the version number is obtained as follows: 256×1+1=257. Enter the IP address of the E5061B in the cell to the right side of "IP Address." This VBA macro will not work properly without the correct values in these two cells.
In part 2, the sweep range (start and stop points) and the number of measurement points are set. Click Set to execute the setting operation as specified with the setting table, while clicking the button labeled "Query" retrieves the current settings of the E5061B.
Part 3 is dedicated to setting the trigger mode.
Part 4 sets the measurement parameters and data format for trace 1 in channel 1. Click Set to execute the setting operation as specified with the setting table, while clicking the button labeled "Query" retrieves the current settings of the E5061B.
In part 5, click Auto Scale to execute auto scaling for trace 1 in channel 1.
Click Read Trace in part 6 to retrieve the formatted data of trace 1 in channel 1. The data is displayed in tabular.
Click Preset to execute the presetting operation.
This section describes the operation of the VBA macro, focusing on the part related to control with WinSock API.
In order to use WinSock API, you must declare functions and define variables with a definition file of WinSock API, as shown in Definition file of WinSock API.
'This is the Winsock API definition file for Visual Basic
'Setup the variable type 'hostent' for the WSAStartup command
Type Hostent
h_name As Long
h_aliases As Long
h_addrtype As String * 2
h_length As String * 2
h_addr_list As Long
End Type
Public Const SZHOSTENT = 16
'Set the Internet address type to a long integer (32-bit)
Type in_addr
s_addr As Long
End Type
'A note to those familiar with the C header file for Winsock
'Visual Basic does not permit a user-defined variable type
'to be used as a return structure. In the case of the
'variable definition below, sin_addr must
'be declared as a long integer rather than the user-defined
'variable type of in_addr.
Type sockaddr_in
sin_family As Integer
sin_port As Integer
sin_addr As Long
sin_zero As String * 8
End Type
Public Const WSADESCRIPTION_LEN = 256
Public Const WSASYS_STATUS_LEN = 128
Public Const WSA_DescriptionSize = WSADESCRIPTION_LEN + 1
Public Const WSA_SysStatusSize = WSASYS_STATUS_LEN + 1
'Setup the structure for the information returned from
'the WSAStartup() function.
Type WSAData
wVersion As Integer
wHighVersion As Integer
szDescription As String * WSA_DescriptionSize
szSystemStatus As String * WSA_SysStatusSize
iMaxSockets As Integer
iMaxUdpDg As Integer
lpVendorInfo As String * 200
End Type
'Define socket return codes
Public Const INVALID_SOCKET = &HFFFF
Public Const SOCKET_ERROR = -1
'Define socket types
Public Const SOCK_STREAM = 1 'Stream socket
Public Const SOCK_DGRAM = 2 'Datagram socket
Public Const SOCK_RAW = 3 'Raw data socket
Public Const SOCK_RDM = 4 'Reliable Delivery socket
Public Const SOCK_SEQPACKET = 5 'Sequenced Packet socket
'Define address families
Public Const AF_UNSPEC = 0 'unspecified
Public Const AF_UNIX = 1 'local to host (pipes, portals)
Public Const AF_INET = 2 'internetwork: UDP, TCP, etc.
Public Const AF_IMPLINK = 3 'arpanet imp addresses
Public Const AF_PUP = 4 'pup protocols: e.g. BSP
Public Const AF_CHAOS = 5 'mit CHAOS protocols
Public Const AF_NS = 6 'XEROX NS protocols
Public Const AF_ISO = 7 'ISO protocols
Public Const AF_OSI = AF_ISO 'OSI is ISO
Public Const AF_ECMA = 8 'european computer manufacturers
Public Const AF_DATAKIT = 9 'datakit protocols
Public Const AF_CCITT = 10 'CCITT protocols, X.25 etc
Public Const AF_SNA = 11 'IBM SNA
Public Const AF_DECnet = 12 'DECnet
Public Const AF_DLI = 13 'Direct data link interface
Public Const AF_LAT = 14 'LAT
Public Const AF_HYLINK = 15 'NSC Hyperchannel
Public Const AF_APPLETALK = 16 'AppleTalk
Public Const AF_NETBIOS = 17 'NetBios-style addresses
Public Const AF_MAX = 18 'Maximum # of address families
'Setup sockaddr data type to store Internet addresses
Type sockaddr
sa_family As Integer
sa_data As String * 14
End Type
Public Const SADDRLEN = 16
'Declare Socket functions
Public Declare Function closesocket Lib "wsock32.dll" (ByVal s As Long) As Long
Public Declare Function connect Lib "wsock32.dll" (ByVal s As Long, addr As sockaddr_in, ByVal namelen As Long) As Long
Public Declare Function htons Lib "wsock32.dll" (ByVal hostshort As Long) As Integer
Public Declare Function inet_addr Lib "wsock32.dll" (ByVal cp As String) As Long
Public Declare Function recv Lib "wsock32.dll" (ByVal s As Long, ByVal buf As Any, ByVal buflen As Long, ByVal flags As Long) As Long
Public Declare Function recvB Lib "wsock32.dll" Alias "recv" (ByVal s As Long, buf As Any, ByVal buflen As Long, ByVal flags As Long) As Long
Public Declare Function send Lib "wsock32.dll" (ByVal s As Long, buf As Any, ByVal buflen As Long, ByVal flags As Long) As Long
Public Declare Function socket Lib "wsock32.dll" (ByVal af As Long, ByVal socktype As Long, ByVal protocol As Long) As Long
Public Declare Function WSAStartup Lib "wsock32.dll" (ByVal wVersionRequired As Long, lpWSAData As WSAData) As Long
Public Declare Function WSACleanup Lib "wsock32.dll" () As Long
Public Declare Function WSAUnhookBlockingHook Lib "wsock32.dll" () As Long
Public Declare Sub CopyMemory Lib "kernel32" Alias "RtlMoveMemory" (hpvDest As Any, hpvSource As Any, ByVal cbCopy As Long)
The basic control flow with WinSock API is shown in the figure below:

The procedures of each step in Control flow with WinSock API are described below.
Startup
The procedure corresponding to Startup is StartIt. StartIt launches and initializes WinSock API with WSAStartup, whose version is shown in part 1 of ctrl_ lan.xls. The function WSAStartup should always be used when initiating WinSock. This function takes the version number (input) and launching information (output) as its parameters.
Sub StartIt()
Dim StartUpInfo As WSAData
'Version 1.1 (1*256 + 1) = 257
'version 2.0 (2*256 + 0) = 512
'Get WinSock version
Sheets("Sheet1").Select
Range("C2").Select
version = ActiveCell.FormulaR1C1
'Initialize Winsock DLL
x = WSAStartup(version, StartUpInfo)
End Sub
The procedure for Socket Creation and Connection is OpenSocket. OpenSocket makes a connection to an instrument associated with the IP address specified with the input parameter Hostname. It uses a socket of the port specified with the input parameter PortNumber. Each functional part of OpenSocket is described below.
In (1), the inet_aadr function of WinSock API is used to convert an IP address delimited by "." to an Internet address.
In (2), a new socket is created with the socket function of WinSock API and its socket descriptor is obtained. If an error occurs, the control returns to the main program with a message. The socket function takes an address family (input), a socket type (input), and a protocol number (input) as its parameters.
In (3), the socket address is specified. Note that htons, which is used for specifying the port number, is a function of WinSock API. This function converts a 2-byte integer from the Windows byte order (little endian) to the network byte order (big endian).
In (4), a connection to the E5061B is made by using the connect function of WinSock API. If an error occurs, the control returns to the main program with a message. The connect function takes a socket descriptor (input), a socket address (input), and the size of the socket address (input) as its parameters.
Function OpenSocket(ByVal Hostname As String, ByVal PortNumber As Intege r) As Integer
Dim I_SocketAddress As sockaddr_in
Dim ipAddress As Long
ipAddress = inet_addr(Hostname) '...........(1)
'Create a new socket
socketId = socket(AF_INET, SOCK_STREAM, 0) '
If socketId = SOCKET_ERROR Then '
MsgBox ("ERROR: socket = " + Str$(socketId)) '...........(2)
OpenSocket = COMMAND_ERROR '
Exit Function '
End If '
'Open a connection to a server
I_SocketAddress.sin_family = AF_INET '
I_SocketAddress.sin_port = htons(PortNumber) '...........(3)
I_SocketAddress.sin_addr = ipAddress '
I_SocketAddress.sin_zero = String$(8, 0) '
x = connect(socketId, I_SocketAddress, Len(I_SocketAddress)) '
If socketId = SOCKET_ERROR Then '
MsgBox ("ERROR: connect = " + Str$(x)) '..(4)
OpenSocket = COMMAND_ERROR '
Exit Function '
End If '
OpenSocket = socketId
End Function
The procedure corresponding to Communication is SendCommand. SendCommand transmits a message (SCPI command) specified with the input parameter "command" to the E5061B using the send function of WinSock API. The send function takes a socket descriptor (input), a message to be transmitted (input), message length (input) and a flag (input) as its parameters.
Function SendCommand(ByVal command As String) As Integer
Dim strSend As String
strSend = command + vbCrLf
count = send(socketId, ByVal strSend, Len(strSend), 0)
If count = SOCKET_ERROR Then
MsgBox ("ERROR: send = " + Str$(count))
SendCommand = COMMAND_ERROR
Exit Function
End If
SendCommand = NO_ERROR
End Function
The procedure corresponding to the Receiving part of communication is RecvAscii and other functions. RecvAscii receives a message in ASCII format and stores it in the dataBuf output parameter. Maximum length of the message is specified with the maxLength input parameter. Each functional part of RecvAscii is described below.
In (1), a message (a response to a query for a SCPI command) is received from the E5061B as a series of characters using the recv function of WinSock API. If an error occurs, the control returns to the main program with a message. The recv function takes a socket descriptor (input), a message to be received (input), message length (input) and a flag (input) as its parameters.
In (2), it is determined whether each received character is LF (ASCII code: 10). When it is LF, receiving is terminated by adding NULL (ASCII code: 0) to the end of the dataBuf string and the control returns to the main program.
In (3), the number of the last characters that were read out is added to the count value for checking the number of received characters, and the characters are appended to the end of the dataBuf string.
Function RecvAscii(dataBuf As String, ByVal maxLength As Integer) As Integer
Dim c As String * 1
Dim length As Integer
dataBuf = ""
While length < maxLength
DoEvents
count = recv(socketId, c, 1, 0) '
If count < 1 Then '
RecvAscii = RECV_ERROR '............(1)
dataBuf = Chr$(0) '
Exit Function '
End If '
If c = Chr$(10) Then '
dataBuf = dataBuf + Chr$(0) '............(2)
RecvAscii = NO_ERROR '
Exit Function '
End If '
length = length + count '............(3)
dataBuf = dataBuf + c '
Wend
RecvAscii = RECV_ERROR
End Function
The procedure corresponding to Disconnection is CloseConnection. CloseConnection disconnects communication and removes a socket using the closesocket function of WinSock API. The closesocket function takes a socket descriptor (input) as its parameter.
Sub CloseConnection()
x = closesocket(socketId)
If x = SOCKET_ERROR Then
MsgBox ("ERROR: closesocket = " + Str$(x))
Exit Sub
End If
End Sub
End
The procedure corresponding to End is EndIt. EndIt disconnects WinSock API using the WSACleanup function of WinSock API. The function WSACleanup should always be used when terminating WinSock.
Sub EndIt()
'Shutdown Winsock DLL
x = WSACleanup()
End Sub
The E5061B can be controlled by executing the above procedures in order, following the control flow in Control flow with WinSock API. This is demonstrated by the procedure autoscale (a procedure that is executed when the Auto Scale button is clicked) as described in autoscale.
Sub autoscale()
'
' auto scaling
'
Call StartIt
Call get_hostname
x = OpenSocket(Hostname$, ScpiPort)
x = SendCommand(":DISP:WIND1:TRAC1:Y:AUTO")
Call CloseConnection
Call EndIt
End Sub
When you execute more than one command by connecting and disconnecting a socket for every command, the sequence of execution may change.