Time Domain

Other topics about Sample Programs

Overview

This sample program demonstrates how to use the transformation function of the time domain function.

This program executes calibration (ECal), performs measurement once, converts the results to data in the time domain, and displays this data.

See Analysis in Time Domain (time domain function) for this programming.

Sample Program in Excel VBA

Private Sub Time_Domain_Click()

    Dim defrm As Long                       'Session to Default Resource Manager

    Dim vi As Long                          'Session to instrument

    Dim Para As String

    Dim Tran_Type As String

    Dim Stim_Type As String

    Dim stop_freq As Double

    Dim Win_Beta As Double

    Dim Star_Time As Double

    Dim Stop_Time As Double

    Dim Result As String

    

    Const TimeOutTime = 40000               'timeout time.

    

    stop_freq = 3000000000#                 'Stop Frequendy  : 3 GHz

    Nop = 201                               'Nop             : 201

    Para = "S11"                            'Meas. Parameter : S11

    Tran_Type = "LPAS"                      'Transform Type  : Lowpass

    Stim_Type = "IMP"                       'Stimulus Type   : Impulse

    Win_Beta = 13                           'Window Beta     : 13 (Maximum Type)

    Star_Time = 0                           'Start time      : 0 sec

    Stop_Time = 0.00000001                  'Stop time       : 10 nsec

    

    Call viOpenDefaultRM(defrm)                                                     'Initializes the VISA system.

    Call viOpen(defrm, "GPIB0::17::INSTR", 0, 0, vi)                                'Opens the session to the specified instrument.

    Call viSetAttribute(vi, VI_ATTR_TMO_VALUE, TimeOutTime)                         'The state of an attribute for the specified session.

    

    Call viVPrintf(vi, ":SYST:PRES" & vbLf, 0)                                      'Presets the setting state of the ENA.

    Call viVPrintf(vi, "*CLS" & vbLf, 0)                                            'Clears the all status register.

    

    Call viVPrintf(vi, ":SENS1:FREQ:STOP " & stop_freq & vbLf, 0)                   'Sets the sweep stop frequency.

    Call viVPrintf(vi, ":SENS1:SWE:POIN " & Nop & vbLf, 0)                          'Sets the number of points.

    

    Call viVPrintf(vi, ":CALC1:TRAN:TIME:LPFR" & vbLf, 0)                           'Sets a measurement point.

    

    Call viVPrintf(vi, ":CALC1:PAR1:DEF " & Para & vbLf, 0)                         'Sets the measurement parameter.

    Call viVPrintf(vi, ":TRIG:SOUR BUS" & vbLf, 0)                                  'Sets the trigger source to BUS.

    Call ErrorCheck(vi)                                                             'Checking the error.

    

    MsgBox "Connect Port1 to Ecal Module. Then click OK button.", vbOKOnly          'Display the message box.

    

    Call viVPrintf(vi, ":SENS1:CORR:COLL:ECAL:SOLT1 1" & vbLf, 0)                   'Execute the 1-port calibration.

    Call viVPrintf(vi, "*OPC?" & vbLf, 0)                                           'Sets the *OPC? command.

    Call viVScanf(vi, "%t", Result)                                                 'Reads the *OPC? result.

    Call ErrorCheck(vi)                                                             'Checking the error.

    MsgBox "Set DUT. Then click OK button.", vbOKOnly                               'Display the message box.

    

    Call viVPrintf(vi, ":TRIG:SING" & vbLf, 0)                                      'Execute the trigger.

    Call viVPrintf(vi, "*OPC?" & vbLf, 0)                                           'Sets the *OPC? command.

    Call viVScanf(vi, "%t", Result)                                                 'Reads the *OPC? result.

    Call viVPrintf(vi, ":DISP:WIND1:TRAC1:Y:AUTO" & vbLf, 0)                        'Execute auto scale.

    

    MsgBox "Click OK button. < Time Domain Transform >", vbOKOnly                   'Display the message box.

    

    Call viVPrintf(vi, ":CALC1:TRAN:TIME " & Tran_Type & vbLf, 0)                   'Sets the transformation type.

    Call viVPrintf(vi, ":CALC1:TRAN:TIME:STIM " & Stim_Type & vbLf, 0)              'Sets the stimulus type.

    Call viVPrintf(vi, ":CALC1:TRAN:TIME:KBES " & Win_Beta & vbLf, 0)               'Sets the beta value of the window.

    Call viVPrintf(vi, ":CALC1:TRAN:TIME:STAR " & Star_Time & vbLf, 0)              'Sets the start value of the display range.

    Call viVPrintf(vi, ":CALC1:TRAN:TIME:STOP " & Stop_Time & vbLf, 0)              'Sets the end value of the display range.

    Call viVPrintf(vi, ":CALC1:TRAN:TIME:STAT ON" & vbLf, 0)                        'Turns on the time domain function.

    Call ErrorCheck(vi)                                                             'Checking the error.

    

    Call viVPrintf(vi, ":CALC1:PAR1:SEL" & vbLf, 0)                                 'Sets the active trace.

    Call viVPrintf(vi, ":CALC1:FORM REAL" & vbLf, 0)                                'Sets the real data format.

    Call viVPrintf(vi, ":DISP:WIND1:TRAC1:Y:AUTO" & vbLf, 0)                        'Execute auto scale.

    Call ErrorCheck(vi)                                                             'Checking the error.

    

    Call viClose(vi)                                                                'Closes the resource manager session.

    Call viClose(defrm)                                                             'Breaks the communication and terminates the VISA system.

    

    End                                                                             'End

End Sub

 

Private Sub EndBtn_Click()

    End

End Sub

 

Sub ErrorCheck(vi)

    Dim err As String * 50, ErrNo As Variant, Response As VbMsgBoxResult

    Call viVQueryf(vi, ":SYST:ERR?" & vbLf, "%t", err)

    ErrNo = Split(err, ",")

    If Val(ErrNo(0)) <> 0 Then

        Response = MsgBox(CStr(ErrNo(1)), vbOKOnly)

    End If

End Sub

 

Sample Program in HT Basic

10 DIM Para$[9],Tran_type$[9],Stim_type$[9],Buff$[9],Inp_ch ar$[9]

20 REAL Stop_freq,Win_beta,Star_time,Stop_time

30 INTEGER Nop

40 !

50 ASSIGN @Agte506x TO 717

60 !

70 Stop_freq=3.E+9 ! Stop Frequency : 3 GHz

80 Nop=201 ! Nop : 201

90 Para$="S11" ! Meas. Parameter : S11

100 !

110 Tran_type$="LPAS" ! Transform Type : Lowpass

120 Stim_type$="IMP" ! Stimulus Type : Impulse

130 Win_beta=13 ! Window Beta : 13 (Maximum Type)

140 Star_time=0 ! Start time : 0 s

150 Stop_time=1.E-8 ! Stop time : 10 ns

160 !

170 OUTPUT @Agte506x;":SYST:PRES"

180 OUTPUT @Agte506x;":SENS1:FREQ:STOP ";Stop_freq

190 OUTPUT @Agte506x;":SENS1:SWE:POIN ";Nop

200 !

210 OUTPUT @Agte506x;":CALC1:TRAN:TIME:LPFR"

220 !

230 OUTPUT @Agte506x;":CALC1:PAR1:DEF "&Para$

240 OUTPUT @Agte506x;":TRIG:SOUR BUS"

250 !

260 ! 1 Port Full Calibration (ECal)

270 !

280 PRINT "Connect Port 1 to ECal Module. Then push [Enter] key."

290 INPUT "",Buff$

300 OUTPUT @Agte506x;":SENS1:CORR:COLL:ECAL:SOLT1 1"

310 OUTPUT @Agte506x;":SYST:ERR?"

320 ENTER @Agte506x;Buff$

330 !

340 ! Measurement

350 !

360 PRINT "Set DUT. Then Push [Enter] key."

370 INPUT "",Inp_char$

380 !

390 OUTPUT @Agte506x;":TRIG:SING"

400 OUTPUT @Agte506x;"*OPC?"

410 ENTER @Agte506x;Buff$

420 !

430 OUTPUT @Agte506x;":DISP:WIND1:TRAC1:Y:AUTO"

440 PRINT "Push [Enter] key. -> [Time Domain Transform]"

450 INPUT "",Inp_char$

460 !

470 ! Time Domain Transform

480 !

490 OUTPUT @Agte506x;":CALC1:TRAN:TIME "&Tran_type$

500 OUTPUT @Agte506x;":CALC1:TRAN:TIME:STIM "&Stim_type$

510 OUTPUT @Agte506x;":CALC1:TRAN:TIME:KBES ";Win_beta

520 OUTPUT @Agte506x;":CALC1:TRAN:TIME:STAR ";Star_time

530 OUTPUT @Agte506x;":CALC1:TRAN:TIME:STOP ";Stop_time

540 OUTPUT @Agte506x;":CALC1:TRAN:TIME:STAT ON"

550 !

560 OUTPUT @Agte506x;":CALC1:PAR1:SEL"

570 OUTPUT @Agte506x;":CALC1:FORM REAL"

580 OUTPUT @Agte506x;":DISP:WIND1:TRAC1:Y:AUTO"

590 END