Other topics about Sample Programs
This sample program demonstrates how to use the :TRIG:SING command to wait until the measurement cycle is completed.
This sample program correctly runs when the maximum number of channels/traces is set to 4 channels/4 traces.
The sample program uses the :TRIG:SING command to start a sweep (measurement) cycle, uses the *OPC command to wait until the measurement cycle is completed, then prints a message and exits.
See Waiting for the End of Measurement for this programming.
Sub trg_sing_Click()
Dim defrm As Long
Dim vi As Long
Dim ContMode(4) As String
Dim Result As String * 10
Dim i As Integer
Const TimeOutTime = 100000 ' TimeOut time should be greater than the measurement time.
'
' Assign a GPIB address to the I/O pass.
Call viOpenDefaultRM(defrm)
Call viOpen(defrm, "GPIB0::17::INSTR", 0, 0, vi)
Call viSetAttribute(vi, VI_ATTR_TMO_VALUE, TimeOutTime)
'
' Store the settings of continuous initiation mode for each channel
' (on for channels 1 and 2; off for channels 3 and 4)
' into the array variable ContMode().
ContMode(1) = "ON"
ContMode(2) = "ON"
ContMode(3) = "OFF"
ContMode(4) = "OFF"
'
' Turn on or off continuous initiation mode for each channel
' depending on the value of ContMode(*).
Call viVPrintf(vi, ":DISP:SPL D12_34" & vbLf, 0)
Call viVPrintf(vi, ":SENS1:SWE:TIME:AUTO OFF" & vbLf, 0)
Call viVPrintf(vi, ":SENS1:SWE:TIME 5" & vbLf, 0)
Call viVPrintf(vi, ":SENS2:SWE:TIME:AUTO OFF" & vbLf, 0)
Call viVPrintf(vi, ":SENS2:SWE:TIME 3" & vbLf, 0)
Call viVPrintf(vi, ":SENS3:SWE:TIME:AUTO OFF" & vbLf, 0)
Call viVPrintf(vi, ":SENS3:SWE:TIME 1" & vbLf, 0)
Call viVPrintf(vi, ":SENS4:SWE:TIME:AUTO OFF" & vbLf, 0)
Call viVPrintf(vi, ":SENS4:SWE:TIME 3" & vbLf, 0)
For i = 1 To 4
Call viVPrintf(vi, ":INIT" & CStr(i) & ":CONT " & ContMode(i) & vbLf, 0)
Next i
' Set the trigger source to Bus Trigger.
Call viVPrintf(vi, ":TRIG:SOUR BUS" & vbLf, 0)
'
' Trigger the instrument to start a sweep cycle.
Call viVPrintf(vi, ":TRIG:SING" & vbLf, 0)
'
' Execute the *OPC? command and wait until the command
' returns 1 (i.e., the measurement cycle is completed).
Call viVPrintf(vi, "*OPC?" & vbLf, 0)
Call viVScanf(vi, "%t", Result)
'
' Display a measurement completion message.
Stat = MsgBox("Measurement complete", vbOKOnly)
Call viClose(vi)
Call viClose(defrm)
End Sub
10 DIM Cont_mode$(1:4)[9],Buff$[9]
20 INTEGER I
30 !
40 ASSIGN @Agte506x TO 717
50 !
60 Cont_mode$(1)="ON"
70 Cont_mode$(2)="ON"
80 Cont_mode$(3)="OFF"
90 Cont_mode$(4)="OFF"
150 !
160 FOR I=1 TO 4
170 OUTPUT @Agte506x;":INIT"&VAL$(I)&":CONT "&Cont_mode$(I)
180 NEXT I
190 OUTPUT @Agte506x;":TRIG:SOUR BUS"
200 !
210 OUTPUT @Agte506x;":TRIG:SING"
220 OUTPUT @Agte506x;"*OPC?"
230 ENTER @Agte506x;Buff$
240 !
250 PRINT "Measurement complete"
260 END