Waiting for End of Measurement (SRQ)

Other topics about Sample Programs

Overview

This sample program demonstrates how to use an SRQ to detect the end of measurement.

The sample program sets up the trigger system, configures the instrument to properly generate an SRQ, and then triggers the instrument. When the instrument has generated an SRQ that indicates the end of measurement, the program exits after printing a measurement completion message.

See Waiting for the End of Measurement for this programming.

Sample Program in Excel VBA

Option Explicit

Implements VisaComLib.IEventHandler

    '*** The variables of the resource manager

    Dim ioMgr As VisaComLib.ResourceManager

    Dim Ena As VisaComLib.FormattedIO488

    Dim SRQ As VisaComLib.IEventManager

Sub IEventHandler_HandleEvent( _

        ByVal Ena As VisaComLib.IEventManager, _

        ByVal SRQevent As VisaComLib.IEvent, _

        ByVal userHandle As Long)

    '* Once the SRQ is detected, then get the data

    Call ReadData

End Sub

Sub UserForm_Initialize()

    '*** Variable declaration.

    Dim i As Double, dummy As Integer

    Range("A5:B500").Clear

    

    '*** Instrument I/O declarlation

    Set ioMgr = New VisaComLib.ResourceManager

    Set Ena = New VisaComLib.FormattedIO488

  

    '*** Open the instrument & Sets the GPIB address

    Set Ena.IO = ioMgr.Open("GPIB0::17::INSTR") ' You can change VISA address

    Ena.IO.timeout = 100000   ' TimeOut time should be greater than the measurement time.

    

    '*** SRQ declarlation

    Set SRQ = Ena.IO

    SRQ.InstallHandler EVENT_SERVICE_REQ, Me

    SRQ.EnableEvent EVENT_SERVICE_REQ, EVENT_HNDLR

    

    '* Clears the operation status event register and the status byte register.

    Ena.WriteString "*CLS", True

    

    '* Aborts the trigger and sets the trigger source to the bus trigger.

    Ena.WriteString ":ABOR", True

    Ena.WriteString ":INIT:CONT ON", True

    Ena.WriteString ":TRIG:SOUR BUS", True

    

    '* Sets the positive transition filter to 0 and the negative transition filter to 1

    '*  so that the operation status event register at bit 4 is set to 1 only when the

    '*  operation status condition register at bit 4 is changed from 1 to 0.

    Ena.WriteString ":STAT:OPER:PTR 0", True

    Ena.WriteString ":STAT:OPER:NTR 16", True

    

    '* Enables bit 4 in the operation status event register and bit 7 in the status byte register.

    Ena.WriteString ":STAT:OPER:ENAB 16", True

    Ena.WriteString "*SRE 128", True

       

End Sub

 Sub CmdTrigger_Click()

    '* Making a trigger

    Ena.WriteString ":TRIG", True

End Sub

 Sub ReadData()

    '* Clear the status register

    Ena.WriteString "*CLS", True

    Range("A5:B500").Clear

    Dim i As Integer

    Dim MeasData As Variant

    '* Get the measurement data.

    Ena.WriteString ":CALC1:DATA:FDAT?", True

    MeasData = Ena.ReadList(ASCIIType_R8, ",")

 

    '* Display the data on the sheet

    ActiveSheet.Cells(6, 1) = "Data (Primary)"

    ActiveSheet.Cells(6, 2) = "Data (Secondary)"

    For i = 1 To UBound(MeasData)

        ActiveSheet.Cells(i + 6, 1).Value = MeasData(i * 2 - 2)

        ActiveSheet.Cells(i + 6, 2).Value = MeasData(i * 2 - 1)

    Next i

End Sub

Sub CmdClose_Click()

    '* Close

    Ena.IO.Close

    Unload Me

End Sub