Other topics about Controlling Peripherals
The following figure shows the flow of controlling the instrument with VISA. When developing a VISA program in the Visual Basic language, a special programing notice (in the readme text file listed below) must be reviewed.
For details on the use of the VISA library and the programing notice for using the VISA library with the E5061B macro (E5061B VBA), refer to the following files contained in I/O library CD-ROM.
visa.hlp (on-line help for the VISA library)
vbreadme.txt (notes on using the VISA library with VB)
To use the VISA library in the E5061B macro (E5061B VBA), you need to import two definition files into your project with the Visual Basic editor to define the VISA functions and perform other tasks. The definition files are stored on the sample programs disk under the following filenames (for information on importing modules, refer to Saving a Module (Exporting).
visa32.bas
Flow of instrument control with VISA
The VISA system startup session is viOpenDefaultRM function in the sample program ctrl_ext.vba. VISA's viOpenDefaultRM function initializes and starts up the VISA system. The viOpenDefaultRM function must be executed before other VISA functions are called, and the parameter of this function has the startup information (Defrm in ctrl_ext.vba).
viOpenDefaultRM(param)
|
Parameter |
(param) |
|
Description |
Startup information (output) |
|
Data type |
Long integer type |
The connection session is viOpen function. VISA's viOpen function makes connection with the specified instrument. The viOpen function returns a value so that the VISA functions can apply it to the specified instrument. The parameters of this function contain the startup information (Defrm), the address information of the specified instrument ("GPIB0::17::INSTR" in ctrl_ext.vba), access mode (0 in ctrl_ext.vba), timeout (0 in ctrl_ext.vba), and connection information (Equip in ctrl_ext.vba).
viOpen(param1, param2, param3, param4, param5)
|
Parameter |
(param1) |
|
Description |
Startup information (input) |
|
Data type |
Long integer type |
|
Parameter |
(param2) |
|
Description |
Address information of the specified instrument (input) |
|
Data type |
Character string type |
|
Syntax |
"GPIB0::gpib address::INSTR" "USB0::manufacturer ID::model code::serial number::0::INSTR" "TCPIP0::IP address::inst0::INSTR" |
|
Parameter |
(param3) |
|
Description |
Access mode (Enter 0) |
|
Parameter |
(param4) |
|
Description |
Timeout (Enter 0) |
|
Parameter |
(param5) |
|
Description |
Connection information (output) |
|
Data type |
Long integer type |
The communication session is viVPrintf function. VISA's viVPrintf function sends a program message (GPIB command) to the specified instrument. The parameters of this function contain the connection information (Equip), the program message (*IDN?), and the variable to be formatted (0 in ctrl_ext.vba).
To input/output GPIB commands, the viVPrintf function and the viVScanf function are mainly used, but other VISA functions are also available. For more information, refer to visa.hlp (online help for the VISA library).
viVPrintf(param1, param2, param3)
|
Parameter |
(param1) |
|
Description |
Connection information (input) |
|
Data type |
Long integer type |
|
Parameter |
(param2) |
|
Description |
Program message (input) When sending a program message of the GPIB command, a message terminator is required at the end of the message (Chr$(10) in ctrl_ext.vba) |
|
Data type |
Character string type |
|
Parameter |
(param3) |
|
Description |
A variable to be formatted. If not applicable, enter 0. |
|
Data type |
Specified data type |
The receiving session is viVScanf function. VISA's viVScanf function receives the result from the specified instrument and stores it in the output variable. The parameters of this function contain the connection information (Equip in ctrl_ext.vba), the format parameter for the output variable (%t in ctrl_ext.vba), and the output variable (Prod in ctrl_ext.vba).
viVScanf(param1, param2, param3)
|
Parameter |
(param1) |
|
Description |
Connection information (input) |
|
Data type |
Long integer type |
|
Parameter |
(param2) |
|
Description |
Format parameter for the output variable |
|
Data type |
Character string type |
|
Parameter |
(param3) |
|
Description |
Output variable (output) |
|
Data type |
Character string type |
The disconnection session is viClose function. VISA's viClose function disconnects communication and terminates the VISA system. The parameter of this function has startup information (Defrm in ctrl_ext.vba).
viClose(param)
|
Parameter |
(param) |
|
Description |
Startup information (input) |
|
Data type |
Long integer type |
The ctrl_ext.vba is a sample program that controls instruments connected through USB/GPIB interface cable using the E5061B as the system controller. This VBA program consists of the following modules.
|
Object name |
Module type |
Content |
|
mdlCtrlExt |
Standard module |
Reads out the product information of external instrument. |
|
Visa32 |
Standard module |
Definition file to use VISA library (Visa32.bas) |
When you control peripherals from E5061B VBA, use the GPIB comĀmands provided for the instrument to communicate with VISA. On the other hand, when you control the E5061B itself with E5061B VBA, use the COM objects provided for the E5061B to communicate.
Read out the product information (ctrl_ext.vba)
''''
' This program is sample of controlling peripherals.
''''
'
Sub Main()
Dim status As Long
Dim Defrm As Long
Dim Equip As Long
Dim Prod As String * 100
'
' Initializes and starts up the VISA system and outputs the startup information to the Defrm variable.
' During this process, if an error occurs, the program goes to the error handling routine.
'
status = viOpenDefaultRM(Defrm)
If (status <> VI_SUCCESS) Then GoTo VisaErrorHandler
'
' Establishes the connection to the external instrument (GPIB address: 17) connected via GPIB and
' outputs the connection information to the Equip variable. During this process, if an error occurs,
' the program goes to the error handling routine.
'
status = viOpen(Defrm, "GPIB0::17::INSTR", 0, 0, Equip)
If (status <> VI_SUCCESS) Then GoTo VisaErrorHandler
'
' Queries the product information of the external instrument connected via USB/GPIB interface cable
' using VISA. During this process, if an error occurs, the program goes to the error handling routine.
'
status = viVPrintf(Equip, "*IDN?" & Chr$(10), 0)
If (status <> VI_SUCCESS) Then GoTo VisaErrorHandler
'
' Retrieves the product information through VISA and outputs it into the Prod variable. Displays the
' read-out result in the message box. During this process, if an error occurs, the program goes to
' the error handling routine.
'
status = viVScanf(Equip, "%t", Prod)
If (status <> VI_SUCCESS) Then GoTo VisaErrorHandler
MsgBox Prod
'
' Breaks the communication and terminates the VISA system.
'
Call viClose(Defrm)
'
GoTo Prog_end
'
' If an error occurs in a VISA function, displays the detail of the error and terminates the program.
'
VisaErrorHandler:
Dim VisaErr As String * 200
Call viStatusDesc(Defrm, status, VisaErr)
MsgBox "Error : " & VisaErr, vbExclamation
Exit Sub
'
Prog_end:
'
End Sub