The E5061B can be connected to external input/output devices such as printer, monitor, keyboard and mouse.
Other topics about Using Windows
A printer can be connected to the E5061B through any USB ports on the front or rear panels. Its driver may be required to install.
A USB mouse and USB keyboard can be connected to the E5061B through any USB ports on the front or rear panels.
A monitor can be connected to the E5061B using the External Monitor Output Terminal (Video) located in the rear panel of the E5061B.
An external monitor needs to be connected to the analyzer and turned ON before the analyzer is turned ON so that the analyzer recognizes the monitor properly.