Other topics about Calibration with ECal
The E5063A allows you to execute ECal calibration with user-defined characteristics instead of the ECal characteristics defined as the factory default. This feature is called User-characterized ECal, and it is used to execute ECal calibration when an adapter is connected to the ECal module.
The E5063A cannot define the User-characterized ECal and cannot save them to the built-in flash memory of the ECal module as the user characteristics. To do that, other ENA network analyzers are required.
The execution procedure for the User-characterized ECal is the same as for normal ECal except that it requires the user characteristics to be selected in advance.
Press Channel Next/Channel Prev keys to select the channel for which you want to execute calibration.
Press Cal > ECal > Characterization.
Select a user characteristic.
To check the information on the user characteristics you have selected, click Characterization Info. The following dialog box appears.

|
1: |
The date when the user characteristics were measured |
|
2: |
The information you entered in Characterization |
|
3: |
The stimulus conditions when the user characteristics were measured |
|
4: |
The information you entered in Adapter Description |
|
5: |
The information you entered in Connectors |