Other topics about Making Measurement
To make a measurement, it is necessary to generate a trigger by using the selected trigger source. Once the internal trigger is selected, a series of triggers is continuously generated as soon as the setting becomes effective.
Pressing Trigger > Restart during a sweep forces the analyzer to abort the sweep.
In a channel, each test port is set to a stimulus port in the order of port number, and updates each trace accordingly.
|
Sweep Order |
Stimulus Port |
Updated Trace |
|
1 |
Port 1 |
S11, S21 |
|
2 |
Port 2 |
S12, S22 |
If full 2-port error correction is in effect, no trace between calibrated ports is updated until the last calibrated port is swept as the stimulus port.
Sweep is not executed for stimulus ports that are not required for updating traces.