Saving the Screen Image to a File

Other topics about Data Output

Overview

Along with printing, the E5063A allows the user to save screen images as bitmap (.bmp) or portable network graphics (.png) files. Saved files can be loaded into PC application software for further processing.

Saving Screen Image as File

Follow the procedure below to save a screen image to a file.

  1. Display the screen to be saved as a file. If you want to save the screen with a white background, set the display mode to inverted display before saving the screen. For details about display mode, see Setting Display Colors.

  2. Press System key. The screen image at the time System key is pressed is the image that will be saved.

  3. Press Dump Screen Image to open the Save As dialog box.

  4. Select the file type from "24-Bit Bitmap (*.bmp)" or "Portable Network Graphics (*.png)".

  5. Select the destination folder and type a file name. (Clicking Input from the front panel on the Save As dialog box activates the on screen keyboard.)

  6. Press Save to save the screen image of E5063A to a file.