Deleting Unnecessary Data in Time Domain (Gating)

Other topics about Time Domain Analysis

Measurement Flow

Item

Description

1. Measurement in frequency domain

Executes measurement in frequency domain

2. Transformation to time domain

Enables transformation function and transforms measurement data to data in time domain

3. Setting the gate

Makes the following settings of the gate to select the necessary domain:

  • Gate type

  • Gate shape

  • Gate range

4. Transformation back to frequency domain

Disables transformation function and displays response in frequency domain corresponding to the data selected with the gate

 

The following figure shows the change in the waveform at each step of the flow.

Setting Gate Type

The E5063A allows you to choose from the following two gate types:

Gate type

Description

Band pass

Deletes response outside the gate range

Notch

Deletes response inside the gate range

Operational procedure

  1. Press Channel Next/Channel Prev and Trace Next/Trace Prev to activate the trace for which you want to set the gate type.

  2. Press Analysis, then click Gating to display the Gating menu.

  3. Click Type to toggle between band pass (Bandpass) and notch (Notch).

Setting Gate Shape

The gate is a filter whose shape looks like a band pass filter. There are several parameters that indicate the gate shape. The following figure shows the definition of the gate shape parameters.

The following table compares the characteristics according to the gate shape. When the shape is "minimum," the cut-off time is shorter and the response is deleted abruptly, but the sidelobe level and band pass ripples become larger. When it is "maximum," cut-off is gentler, but the sidelobe level and the band pass ripple become smaller. The minimum gate span in the following table is the minimum gate range you can set. This value is defined as the minimum gate span necessary for the existence of the pass band and is equal to 2 times the cut-off time.

Gate shape

Passband ripple

Sidelobe level

Cutoff time

Minimum gate span

Minimum

± 0.13 dB

- 48 dB

1.4/frequency span

2.8/frequency span

Normal

± 0.01 dB

- 68 dB

2.8/frequency span

5.6/frequency span

Wide

± 0.01 dB

- 57 dB

4.4/frequency span

8.8/frequency span

Maximum

± 0.01 dB

- 70 dB

12.7/frequency span

25.4/frequency span

Operational procedure

  1. Press  Channel Next/Channel Prev and Trace Next/Trace Prev to activate the trace for which you want to set the gate shape.

  2. Press Analysis, then click Gating to display the Gating menu.

  3. Press Shape and then select the gate shape.

Setting Gate Range

Specify the gate range in time. The ends of the range are defined as the - 6 dB attenuation points shown in the figure above. You can set the gate range by specifying the start and stop times or the center and span. The E5063A has the following limitations on the gate range you can set.

Lower limit     -Tspan   

Upper limit     Tspan

Tspan is the measurement range expressed in time obtained in Measurement range.

Operational procedure

  1. Press Channel Next/Channel Prev and Trace Next/Trace Prev to activate the trace for which you want to set the gate range.

  2. Press Analysis, then click Gating to display the "Gating" menu.

  3. Press each of the following softkeys to specify the gate range. Distance corresponding to the setting time is displayed at the side of the set value area in the data entry bar. The displayed distance is a value that takes the velocity factor into consideration.

Softkey

Function

Start

Sets the start time

Stop

Sets the stop time

Center

Sets the center of the gate in time

Span

Sets the gate span in time

Setting Unit for X-Axis

 Operational procedure

  1. Press Channel Next/Channel Prev and Trace Next/Trace Prev to activate the trace for which you want to set the gate range.

  2. Press Analysis, then click Gating to display the "Gating" menu.

  3. Click Units. The following options are available. These options will represent the X-axis of the graph. Meters, feet and inches are calculated by taking velocity factor into consideration.

Softkey

Function

Seconds

Sets the x-axis to seconds.

Meter

Sets the x-axis to meter (distance).

Feet

Sets the x-axis to feet (distance).

Inches

Sets the x-axis to inches (distance).

Enabling Gating Function

When you enable the gating function, data within the specified range is deleted. When the transformation function is enabled, the flags indicating the gate range is displayed as shown in the following figure.

Operational procedure

  1. Press Channel Next/Channel Prev keys and Trace Next/Trace prev keys to activate the trace for which you want to use the gate function.

  2. Press Analysis key, then click Gating to display the "Gating" menu.

  3. Use Gating to enable (ON) the gate function.