Other topics about Maintenance
User can update E5063A firmware by themselves. The latest firmware can be downloaded from the http://www.keysight.com/find/ena_support.
Updating firmware does not include the following software update.
Windows Operating System
Driver for Windows
Calibration Constant Data
Press System > Service Menu > Exit to terminate the E5063A application.
Download the latest firmware from the download site. (E5063.exe). f you use your local PC to download, save the file to a USB mass storage device in order to move it to E5063A, then connect the USB mass storage device into the front USB port of the E5063A.
Double click E5063.exe to install the firmware.
Follow the instruction of windows installer. After the installation is finished, the instrument restarts.
Press System > Firmware Revision to confirm the firmware revision you have just installed.
Download the latest firmware from the download site. It is prepared as execution file (E5063A_xx.xx.exe).
Run the E5063A_xx.xx.exe to extract the E5063.msi.
If you use your local PC to download, save the file to a USB mass storage device in order to move it to E5063A, then connect the USB mass storage device into the front USB port of the E5063A.
Press System > Service Menu > Update Firmware.
In Open dialog box, select E5063.msi, then press Open. Then the windows installer appears.
Follow the instruction of windows installer. After the installation is finished, the instrument restarts.
Press System > Firmware Revision to confirm the firmware revision you have just installed.