Command/Query
:CALCulate<Ch>[:SELected]:FUNCtion:DOMain:STARt <Value>
:CALCulate<Ch>[:SELected]:FUNCtion:DOMain:STARt?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:FUNCtion:DOMain:STARt <Value>
:CALCulate<Ch>:TRACe<Tr>:FUNCtion:DOMain:STARt?
This command sets/gets the start value of the analysis range.
When the trace coupling is OFF, the active trace or selected trace is the target to be set.
|
Parameter |
Value |
|
Description |
Start value of the analysis range |
|
Data Type |
Numeric type (Real) |
|
Range |
-500G to 500G |
|
Preset Value |
0 |
|
Unit |
Hz (hertz), or s (second) |
{numeric}<newline><^END>
See Peak Search
No equivalent key is available on the front panel.
SCPI.CALCULATE(Ch).SELECTED.FUNCTION.DOMAIN.START
SCPI.CALCULATE(Ch).TRACE(Tr).FUNCTION.DOMAIN.START