:CALC<Ch>:FUNC:POIN

Type

Query

Syntax

:CALCulate<Ch>[:SELected]:FUNCtion:POINts?

 

The following syntax is also supported:

:CALCulate<Ch>:TRACe<Tr>:FUNCtion:POINts?

Description

This command gets number of data pair in :CALC:FUNC:DATA

Variable

Query Response

{numeric}<newline><^END>

Examples

See Peak Search.

Related Commands

:CALC:FUNC:DATA

:CALC:FUNC:EXEC

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.CALCULATE(Ch).SELECTED.FUNCTION.POINTS

SCPI.CALCULATE(Ch).TRACE(Tr).FUNCTION.POINTS