Command/Query
:CALCulate<Ch>[:SELected]:FUNCtion:PPOLarity {POSitive|NEGative|BOTH}
:CALCulate<Ch>[:SELected]:FUNCtion:PPOLarity?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:FUNCtion:PPOLarity {POSitive|NEGative|BOTH}
:CALCulate<Ch>:TRACe<Tr>:FUNCtion:PPOLarity?
This command sets/gets the polarity when performing the peak search with :CALC:FUNC:EXEC.
|
Parameter |
Selection Option |
|
Description |
Polarity for peak search |
|
Data Type |
Character string type (String) |
|
Range |
"POSitive": Positive peak. "NEGative": Negative peak. "BOTH":Both the positive peak and the negative peak. |
|
Preset Value |
POSitive |
{POS|NEG|BOTH}<newline><^END>
See Peak Search.
No equivalent key is available on the front panel.
SCPI.CALCULATE(Ch).SELECTED.FUNCTION.PPOLARITY
SCPI.CALCULATE(Ch).TRACE(Tr).FUNCTION.PPOLARITY