Command
:CALCulate<Ch>[:SELected]:MARKer<Mk>:FUNCtion:EXECute
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:MARKer<Mk>:FUNCtion:EXECute
This command executes the marker search.
See Peak Search.
Marker Search > Max | Min
Marker Search > Peak > Search Peak
Marker Search > Target > Search Target
Marker Search > Multi Peak > Search Multi Peak
Marker Search > Multi Target > Search Multi Target
These softkeys operation can be done by the following two commands:
Max/Min/Peak/Target :CALC:MARK:FUNC:TYPE and :CALC:MARK:FUNC:EXEC.
Multi Peak/Multi Target :CALC:MARK:FUNC:MULT:TYPE and :CALC:MARK:FUNC:EXEC.
SCPI.CALCULATE(Ch).SELECTED.MARKER(Mk).FUNCTION.EXECUTE
SCPI.CALCULATE(Ch).TRACE(Tr).MARKER(Mk).FUNCTION.EXECUTE