Command/Query
:CALCulate<Ch>[:SELected]:TRANsform:DISTance:STIMulus {IMPulse|STEP}
:CALCulate<Ch>[:SELected]:TRANsform:DISTance:STIMulus?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:TRANsform:DISTance:STIMulus {IMPulse|STEP}
:CALCulate<Ch>:TRACe<Tr>:TRANsform:DISTance:STIMulus?
This command sets/gets the stimulus type used for the transformation function of the fault location display. Use :CALC:TRAN:TIME:STIM when :CALC:TRAN:METH is set at time.
|
Parameter |
Selection Option |
|
Description |
The stimulus type |
|
Data Type |
Character string type (String) |
|
Range |
"IMPulse": Specifies the impulse "STEP": Specifies the step |
|
Preset Value |
"IMPulse" |
{IMP|STEP}<newline><^END>
Dim Var as String
Var= "IMPulse"
Ena.WriteString ":CALC1:TRAN:DIST:STIM " & Var, True
Ena.WriteString ":CALC1:TRAN:DIST:STIM?", True
Var=Ena.ReadString
Analysis > Transform > Type > Bandpass | Lowpass Step | Lowpass Imp
SCPI.CALCULATE(Ch).SELECTED.TRANSFORM.DISTANCE.STIMULUS
SCPI.CALCULATE(Ch).TRACE(Tr).TRANSFORM.DISTANCE.STIMULUS