Command/Query
:CALCulate<Ch>[:SELected]:TRANsform:TIME:STEP:RTIMe <Value>
:CALCulate<Ch>[:SELected]:TRANsform:TIME:STEP:RTIMe?
The following syntax is also supported:
:CALCulate<Ch>:TRACe<Tr>:TRANsform:TIME:STEP:RTIMe <Value>
:CALCulate<Ch>:TRACe<Tr>:TRANsform:TIME:STEP:RTIMe?
This command sets/gets the shape of the Kayser Bessel window using the rise time of step signal used for the transformation function of the time domain function. Use :CALC:TRAN:DIST:STEP:RTIM when :CALC:TRAN:METH is set at distance.
|
Parameter |
Value |
|
Description |
The rise time of step signal |
|
Data Type |
Numeric type (Real) |
|
Range |
Varies depending on the frequency span |
|
Preset Value |
54.7833333333p |
|
Unit |
s (second) |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
{numeric}<newline><^END>
Dim Var as Double
Ena.WriteString ":CALC1:TRAN:TIME:STEP:RTIM " & Str(Var), True
Ena.WriteString ":CALC1:TRAN:TIME:STEP:RTIM?", True
Var=Ena.ReadNumber
Analysis > Transform > Window > Step Rise
SCPI.CALCULATE(Ch).SELECTED.TRANSFORM.TIME.STEP.RTIME
SCPI.CALCULATE(Ch).TRACE(Tr).TRANSFORM.TIME.STEP.RTIME