*IDN

Type

Query

Syntax

*IDN?

Description

This command reads the product information (manufacturer, model number, serial number, and firmware revision number) of the E5063A.

:SYST:PERS:MAN and :SYST:PERS:MOD allow you to change the manufacturer name and model number.

Variable

Query Response

{string 1},{string 2},{string 3},{string 4}<newline><^END>

Examples

Dim Var as String
Ena.WriteString "*IDN?", True
Var=Ena.ReadString

Related Commands

*OPT

:SYST:PERS:MAN

:SYST:PERS:MOD

Equivalent Softkey

System > Firmware Revision

COM Command Syntax (Internal Control Only)

SCPI.IEEE4882.IDN