Query
*OPT?
This command reads the identification numbers of options installed in the E5063A.
{String}<newline><^END>
Option number with "," separator (Example: "285, 011")
Dim Var as String
Ena.WriteString "*OPT?", True
Var=Ena.ReadString
System > Firmware Revision
SCPI.IEEE4882.OPT