Command
*TRG
This command triggers the E5063A if the trigger source is set to Bus.
Ena.WriteString "*TRG", True
:TRIG:SOUR
:TRIG:SING
:TRIG
No equivalent key is available on the front panel.
SCPI.IEEE4882.TRG