:TRIG

Type

Command

Syntax

:TRIGger[:SEQuence][:IMMediate]

Description

This command generates a trigger immediately and executes a measurement, regardless of the setting of the trigger mode.  

This command is different from :TRIG:SING as the execution of the object finishes at the time of a trigger.

      • If you execute this object when the trigger system is not in the trigger wait state (trigger event detection state), an error occurs when executed and the object is ignored.

Examples

Ena.WriteString ":TRIG", True

Related Commands

:TRIG:SOUR

:TRIG:SING

*TRG

Equivalent Softkey

Trigger > Trigger (This is for manual trigger.)

COM Command Syntax (Internal Control Only)

SCPI.TRIGGER.SEQUENCE.IMMEDIATE