Command/Query
:SENSe<Ch>:CORRection:COLLect:CKIT:ORDer:SELect <Value>
:SENSe<Ch>:CORRection:COLLect:CKIT:ORDer:SELect?
This command sets/gets a subclass number in the subclass menu.
If the standard number is 0, the standard is invalid for the subclass.
Parameter |
Value |
Description |
The number of the standard subclass. |
Data Type |
Numeric type (Integer) |
Range |
1 ~ 30 |
Preset Value |
1 |
{numeric}<newline><^END>
Dim Var as Long
Var= 5
Ena.WriteString ":SENS1:CORR:COLL:CKIT:ORD:SEL " & Str(Var), True
Ena.WriteString ":SENS1:CORR:COLL:CKIT:ORD:SEL?", True
Var=Ena.ReadNumber
Cal > Modify Cal Kit > Specify CLSs > Sub Class
SCPI.SENSE(Ch).CORRECTION.COLLECT.CKIT.ORDER.SELECT