:SENS<Ch>:CORR:COLL:ECAL:INF

Type

Query

Syntax

:SENSe<Ch>:CORRection:COLLect:ECAL:INFormation?

Description

This command gets the information of the connected ECal module.

Variable

The command return information in a string variable <param> in the following syntax:

Query Response

{String}<newline><^END>

Examples

Dim Var as String
Ena.WriteString ":SENS1:CORR:COLL:ECAL:INF?", True
Var=Ena.ReadString

Related Commands

:SENS:CORR:COLL:SAVE

:SENS:CORR:TYPE

Equivalent Softkey

No equivalent key is available on the front panel.

COM Command Syntax (Internal Control Only)

SCPI.SENSE(Ch).CORRECTION.COLLECT.ECAL.INFORMATION