Command/Query
:SENSe:FREQuency:STOP <Value>
:SENSe:FREQuency:STOP?
This command sets the stop value of the sweep range in the S-parameter measurement.
|
Parameter |
Value |
|
Description |
Stop value |
|
Data Type |
Numeric type (Real) |
|
Range |
See the settable frequency range |
|
Preset Value |
Depending on frequency option. |
|
Unit |
Hz (hertz) |
|
Resolution |
1000m |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
{numeric}<newline><^END>
Dim Var as Double
Var= 50000
Ena.WriteString ":SENS:FREQ:STOP " & Str(Var), True
Ena.WriteString ":SENS:FREQ:STOP?", True
Var=Ena.ReadNumber
Edit Test > Edit Measurement > Measure : S-Parameter > Stop