Types of remote control system

Depending on the system controller and the interface, you can configure 5 types of remote control system as shown in the table below.

System controller

Interface

Overview

External controller (external computer such as PC and workstation)

GPIB
(talker/listener mode)

System to control the E5063A and other devices connected via GPIB from the external controller.
For more information, refer to GPIB remote control system.

LAN

System to control the E5063A and other devices connected via LAN from the external controller.
For more information, refer to LAN remote control system.

USB

System to control the E5063A and other devices connected via USB from the external controller.
For more information, refer to USB Remote Control System.

E5063A

None (Internal Connection)

System to control the E5063A itself using VB Script.

GPIB
(system controller mode)

Not supported

Other topics about Overview