Other topics about Sample Application Program
This section explains how to control the E5063A by using SICL in the Windows environment.
To control the E5063A using the SICL-LAN server, you need to make the preparations described in Control over SICL-LAN server.
Opening ctrl_lansicl.xls in Microsoft Excel displays a screen as shown in the figure below:

For how to use each element in ctrl_lansicl.xls, refer to the following description.
In part 1, in the cell to the right of the SICL-LAN Address, enter the address of the E5063A for control with the SICL-LAN server. This address is XX, which has been set with the command System > Misc Setup > Network Setup > SICL-LAN Address [XX]. Enter the IP address of the E5063A in the cell to the right of the IP Address. This VBA macro will not work properly without the correct values in these two cells.
Click Preset in part 2 to execute the presetting operation.
In part 3, the sweep range (start and stop points) and the number of measurement points for channel 1 are set. Click Set to execute the setting as shown in the setting table.
Part 4 sets the measurement parameters and data format for trace 1 in channel 1. Click Set to execute the setting as shown in the setting table.
Click Read Trace in part 5 retrieves the formatted data array of trace 1 in channel 1. The data is displayed in tabular.
This section describes the operation of the VBA macro, focusing on the part related to control with SICL.
In order to use SICL in your VBA macro, you must declare functions and define variables with a SICL definition file (for VB).
In the VBA macro, ctrl_sicllan.xls, the standard module whose object name is "SICL," is the definition file.
The basic control flow with SICL is shown in Flow of control using SICL.
In this sample program, the ivprintf function, the ivscanf function, and the iread function are used in its communication part; you can use other SICL functions as well. For details, refer to sicl.hlp (the online help of SICL).

For more information on how to use each function of SICL, refer to the SICL manual.
The procedures of each step in Flow of control using SICL are described below.
The procedure corresponding to connection is OpenSession (OpenSession). OpenSession establishes a connection to the E5063A with the iopen function of SICL, using the SICL-LAN Address and IP Address entered in part 1 in ctrl_lansicl.xls. The iopen function takes the address information of the E5063A you specify as its parameters.
Syntax
addr = iopen(dev)
|
Variable |
addr |
|
Description |
Session information (output) |
|
Data type |
Integer type |
|
|
dev |
|
Description |
Address information of the instrument you specify (input) |
|
Data type |
Character string type |
|
Grammar |
sicl-name [ip-address]:interface, sicl-lan-address |
For example, if the parameter (dev) is "lan[192.168.0.1]:hpib9,17," connection is made to the address of 17 of the interface of hpib9 with the E5063A whose IP address is 192.168.0.1 by using the external controller whose SICL interface name is lan.
Function OpenSession() As Integer
Dim ServAddr As String
Dim IpAddr As String
On Error GoTo ErrHandler
'''Get Sicl-Lan Address
Sheets("Sheet1").Select
Range("C2").Select
ServAddr = ActiveCell.FormulaR1C1
'''Get Ip Address
Sheets("Sheet1").Select
Range("C3").Select
IpAddr = ActiveCell.FormulaR1C1
OpenSession = iopen("lan[" & IpAddr & "]:hpib9," & ServAddr)
Call itimeout(OpenSession, 10000)
Exit Function
ErrHandler:
MsgBox "*** Error : " & Error$
Call siclcleanup
End
End Function
The procedure corresponding to sending in communication is OutputSiclLan. OutputSiclLan uses the ivprintf function of SICL to send messages (SCPI commands). The ivprintf function takes the session information output from the iopen function and a program message as its parameters.
Syntax
Status = ivprintf(addr,mes)
|
Status |
|
|
Description |
Return value of the function (output) |
|
Data type |
Integer type |
|
|
addr |
|
Description |
Session information (input) |
|
Data type |
Integer type |
|
|
mes |
|
Description |
|
|
Data type |
Character string type |
Sub OutputSiclLan(addr As Integer, message As String)
Dim Status As Integer
Dim actualcnt As Long
Dim length As Long
On Error GoTo ErrHandler
length = Len(message)
Status = ivprintf(addr, message & Chr$(10))
Exit Sub
ErrHandler:
MsgBox "*** Error : " & Error$
Call siclcleanup
End
End Sub
The procedure corresponding to receiving ASCII format messages in communication is EnterSiclLan. EnterSiclLan uses the ivscanf function of SICL to receive a message in ASCII format and store it into the output variable. The ivscanf function takes the session information output from the iopen function, the format for output, and the data to be output as its parameters.
Syntax
Status = ivscanf(addr,fmt,ap)
|
Variable |
fmt |
|
Description |
Format for output (input) |
|
Data type |
Character string type |
|
|
ap |
|
Description |
Data to be output (output) |
|
Data type |
Character string type |
For information on the variable (Status) and the variable (addr), refer to Variable.
In Visual Basic, variables must be declared as a fixed-length string when receiving string data using the ivscanf function.
Sub EnterSiclLan(addr As Integer, Query As String)
Dim Status As Integer
Dim actualcnt As Long
Dim res As String * 256
On Error GoTo ErrHandler
Status = ivscanf(addr, "%t", res)
Query = Trim(res)
Exit Sub
ErrHandler:
MsgBox "*** Error : " & Error$
Call siclcleanup
End
End Sub
The procedure corresponding to receiving array data in communication is EnterSiclLanArrayReal64, which uses the iread function of SICL to receive array data in the IEEE 64-bit floating point binary transfer format and store it into the output variable. The iread function takes the session information output from the iopen function, the data to be output, the number of data bytes, the condition to finish reading data, and the number of data bytes actually read out as its parameters.
Syntax
Status = iread(addr,buf,bufsize,reason,actual)
|
Variable |
buf |
|
Description |
Data to be output (output) |
|
Data type |
Character string type |
|
|
bufsize |
|
Description |
The number of data bytes (input) |
|
Data type |
Long integer type |
|
|
reason |
|
Description |
The condition to finish reading out data (input) |
|
Data type |
Integer type |
|
|
actual |
|
Description |
The number of data bytes actually read out (output) |
|
Data type |
Long integer type |
For information on the variable (Status) and the variable (addr), refer to Variable.
Each functional of EnterSiclLanArrayReal64 is described below.
(1) Retrieves the data header.
(2) Stores the number of data bytes into the size variable in the header part.
(3) Retrieves the formatted data array for trace 1 in channel 1 and stores it into the databuf variable.
(4) Retrieves the message terminator at the end of the data.
Function EnterSiclLanArrayReal64(addr As Integer, databuf() As Double) As Long
Dim Status As Integer
Dim actualcnt As Long
Dim buf As String * 8
Dim size As Long
On Error GoTo ErrHandler
'''Read header info of "#6NNNNNN"
Status = iread(addr, buf, 8, I_TERM_MAXCNT, actualcnt) '.................(1)
size = Val(Mid$(buf, 3, 6)) '.................(2)
'''Read data
Status = iread(addr, databuf, size, I_TERM_MAXCNT, actualcnt) '.................(3)
'''Read ending LF
Status = iread(addr, buf, 1, I_TERM_MAXCNT, actualcnt) '.................(4)
EnterSiclLanArrayReal64 = size / 8
Exit Function
ErrHandler:
MsgBox "*** Error : " & Error$
Call siclcleanup
End
End Function
The iclose function of SICL is used to disconnect communication. The iclose function takes the session information output from the iopen function as its parameter.
Syntax
Status = iclose(addr)
For information on the variable (Status) and the variable (addr), refer to Variable
The E5063A can be controlled by executing the above procedures in order, following the control flow in Flow of control using SICL. This is demonstrated by the Preset procedure (a procedure that is executed when the Preset button is clicked) as described in Preset.
Sub Preset()
''' Open Session
E506x = OpenSession
'''Presetting the analyzer
Call OutputSiclLan(E506x, ":SYST:PRES")
'''Close Session
Call iclose(E506x)
End Sub