Other topics about Saving and Recalling
To create a directory (folder), use the following command:
To delete a file or a directory, use the following command:
To copy a file, use the following command:
File transfer from the external controller to the E5063A is possible by reading data from a file on the controller and then writing them to the file on the E5063A.
Also, file transfer from the E5063A to the external controller can be possible by reading data from a file on the E5063A using the commands as query and then writing them to the file on the controller.
To retrieve information for the storage that is built in the E5063A (usage, property of file located in a specified directory), use the following command;
See the Transferring Files.