Transformation to time domain

Other topics about Time Domain Analysis

Overview

The transformation function lets you transform a response in the frequency domain to the corresponding response in the time domain.

Measurement Flow

Item

Description

Selecting a type

Selects the transformation type from the following.

Band pass mode

You can set the sweep range arbitrarily. This is suitable for devices through which signals within a certain frequency range pass such as filters.

Low pass mode

Simulates the TDR measurement. This mode is suitable for devices through which dc current or signals of many frequencies pass, such as cables.

The low pass mode provides two types of modes: low pass step and low pass impulse.

Setting the window

Sets the window to reduce the ringing phenomenon, in which a waveform's waves are caused due to the fact that the frequency domain is finite.

Calculating necessary measurement conditions

Calculates the following values to obtain the necessary resolution and measurement range in the time domain.

Sweep range

Number of points

Window width

Setting the frequency range and the number of points

Sets the sweep range and the number of points to the values calculated above.

Setting display range

Sets the range displayed on the graph.

Enabling transformation function

Enables the transformation function.

Selecting a type

There are two types of transformation to the time domain: band pass and low pass. The appropriate transformation type depends on the DUT.

Comparison between band pass mode and low pass mode

Item

Band pass

Low pass

Appropriate DUT

DUTs that do not operate with dc current such as band pass filters.

DUTs that operate with dc current such as cables.

Input signal

You can simulate the response to the impulse signal.

You can simulate the TDR measurement. You can simulate the response to both the impulse signal and step signal.

Selection of the sweep range

You can select the sweep range arbitrarily.

Because dc data are estimated from the first few points, the frequencies of measurement points must be multiples of the start frequency.

Transmission/

reflection measurement

You can perform both transmission and reflection measurements.

You can perform both transmission and reflection measurements.

Identification of mismatches

You can identify the locations of mismatches.

You can identify the locations of mismatches and the type of impedance (capacitive or inductive).

Resolution

 

The resolution in the time domain increases by two times over that in the band pass mode.

Available data format

  • Liner magnitude format

    • In the reflection measurement, it indicates the mean of the reflection coefficient within the frequency sweep range.

    • In the transmission measurement, it indicates the mean of the transmission coefficient within the frequency sweep range.

  • Log magnitude format

    • In the reflection measurement, it indicates the mean of the return loss within the frequency sweep range.

    • In the transmission measurement, it indicates the mean of the transmission gain within the frequency sweep range.

  • SWR format

    • In the reflection measurement, it indicates the mean of SWR (standing wave ratio) within the frequency sweep range.

 

Real format

In the low pass mode, the real format is useful because the time axis data do not have phase information.

Impulse signal and step signal

The E5071C lets you simulate the response from the DUT to two types of signals: impulse signal and step signal. The impulse signal is a pulse-shape signal in which the voltage rises from 0 to a certain value and returns to 0 again. The pulse width depends on the frequency sweep range. The step signal is a signal in which the voltage rises from 0 to a certain value. The rise time depends on the maximum frequency within the frequency sweep range.

Step signal and impulse signal

 

Operation

  1. Press Channel Next/Channel Prev keys and Trace Next/Trace prev keys to activate a trace for which you want to set the transformation type.

  2. Press Analysis key, then click Transform to display the Transform menu.

  3. Type and then press one of the softkeys to specify the type.

  4. Press Format key to display the "Format" menu and then select the data format.

Setting the window

Because the E5071C transforms data within a finite frequency domain to data in the time domain, an unnatural change of data at the end points within the frequency domain occurs. For this reason, the following phenomena occur.

By using the window function, you can lower the level of sidelobes. However, the width of the impulse and the rise time of the step become larger as a penalty. You can select from three types of windows: maximum, normal, and minimum. The following table shows the approximate relation between the window and the sidelobe/impulse width.

Window

Sidelobe level of impulse signal

Width of impulse (50% in low pass mode)

Sidelobe level of step signal

Rise time of step signal (10 -  90%)

Minimum

- 13 dB

0.60/frequency span

- 21 dB

0.45/frequency span

Normal

- 44 dB

0.98/frequency span

- 60 dB

0.99/frequency span

Maximum

- 75 dB

1.39/frequency span

- 70 dB

1.466/frequency span

 

The window function is available only when the response in the time domain is displayed. It does not have any effect when the response in frequency domain is displayed. The following figure shows the effect of the window when measuring the reflection of a short circuit in the time domain.

 

Operation

  1. Press Channel Next/Channel Prev keys and Trace Next/Trace prev keys to activate a trace for which you want to set the window.

  2. Press Analysis key, then click Transform to display the Transform menu.

  3. Press Window and then select a window type.
     

    Softkey

    Function

    Maximum

    Sets the window type to maximum. b  of the Kaiser Bessel function is set to 13.

    Normal

    Sets the window type to normal. b  of the Kaiser Bessel function is set to 6.

    Minimum

    Sets the window type to minimum. b  of the Kaiser Bessel function is set to 0.

    Rise Time

    Sets the window by specifying the impulse width or the step rise time. The lower limit can be set to the value when the window is the minimum, the upper limit when the window is the maximum.

    Kaiser Beta

    Sets the window by specifying the b  value of the Kaiser Bessel function. The Kaiser Bessel function determines the shape of the window. The allowable setting range is 0 to 13.

  4. By specifying Kaiser Beta, Impulse Width, or Rise Time, you can specify a window that is not classified into the three window types. Conversely, when you specify a window type, these values are set automatically.

Calculating necessary measurement conditions

To use the transformation function efficiently, you need to make the following three settings appropriately.

This section describes the details of these settings.

Effect of frequency sweep range on response resolution

The following figure shows an example when measuring the same cable while changing the sweep span. When measured in a narrower sweep range, the overlap between two peaks is larger than when measured in a wider sweep range. By performing measurement in a wider sweep range, adjacent peaks can be clearly separated, which means that the response resolution is smaller.

Effect of frequency sweep range on resolution

The sweep range affects the width of the impulse signal and the rise time of the step signal. The width of the impulse signal and the rise time of the step signal are inversely proportional to the sweep range. Therefore, the wider the sweep range is, the shorter these times are.

The resolution is equal to the width defined at the point of 50% of the impulse signal or the rise time defined at the points of 10% and 90% of the step signal.

Definitions of impulse width and step rise time

 

Effect of the window function on the response resolution

Lowering the sidelobe level with the window function elongates the width of the impulse signal and the rise time of the step signal. As described in Effect of frequency sweep range on response resolution, because the response resolution is equal to the width of the impulse signal and the rise time of the step signal, lowering the sidelobe level enlarges the response resolution. The following table shows the approximate relationship between the response resolution and the window setting.

Correspondence of Window setting and response resolution

Window

Low pass step

Low pass impulse

Band pass

Minimum

0.45/stop frequency

0.60/stop frequency

1.20/frequency span

Normal

0.99/stop frequency

0.98/stop frequency

1.95/frequency span

Maximum

1.46/stop frequency

1.39/stop frequency

2.77/frequency span

The following figure shows how the response changes as the window shape changes. If the magnitudes of adjacent peaks are comparable, you need to make the resolution higher; if they differ significantly, you need to set the window so that smaller peaks with lower sidelobes appear.

Effect of window on response resolution

Effect of the transformation type on the response resolution

Although both transformation types, band pass and low pass impulse, simulate the response of the impulse signal, the impulse width in the low pass impulse mode is half the width of that in the band pass mode as shown in the table above. Therefore, the resolution is better in the low pass mode. If the DUT can be measured in the low pass mode, response data with better resolution is obtained in the low pass mode.

Measurement range

In the time domain function, the measurement range means the range within which the response can be measured without repetition. The repetition of the response occurs because measurement in the frequency domain is performed discretely instead of continuously. The measurement range is inversely proportional to the frequency difference between adjacent measurement points. The frequency difference between measurement points Delta F is expressed as follows by using the span of the sweep frequency Fspan and the number of points  Nmeas.

Therefore, the measurement range is proportional to the number of points-1 and inversely proportional to the span of the sweep range. To enlarge the measurement range, use one of the following methods:

The sweep range is expressed as time or distance. The time of the measurement range  Tspanis as follows:

The distance of the measurement range Lspan is expressed as follows using the velocity factor V and the speed of light in a vacuum c (3*E8 m/s).

The velocity factor varies depending on the material through which the signal propagates: 0.66 for polyethylene and 0.7 for PTFE.

Changes in the settings and the changes in the response

The following table shows the effect of changes in the measurement conditions on the response resolution and the measurement range.

Change in setting

Response resolution

Measurement range

Sidelobe

Widening the sweep range

Becomes smaller

Becomes narrower

Does not change

Setting the window type to maximum

Becomes larger

Does not change

Becomes lower

Increasing the number of points

Does not change

Becomes wider

Does not change

Setting the frequency range and the number of points

Operation

  1. Press Channel Next/Channel Prev keys to activate the channel you want to set.  The frequency range and the number of points are common to all of the traces in the channel. If you want to use different settings, make them on another channel.

  2. Press Sweep Setup key, then press Sweep Type > Lin Freq to set the sweep type to linear sweep.  When the sweep type is set to other than the linear sweep, the time domain function is not available.

  3. Set the sweep range using the Start/Stop or Center/Span keys.

  4. Press Sweep Setup key, then press Points and then enter the number of points. When performing measurement in the low pass mode, press Analysis > Transform > Set Freq Low Pass to adjust the frequency range so that it is appropriate for the low pass mode. The frequency changes depending on the stop frequency as shown below.
     

    Condition of stop frequency

    Frequency setting

    >= Flow * the number of points

    Start frequency = stop frequency/number of points

    < Flow * the number of points

    Start frequency: Flow

    Stop frequency = Flow * Number of points

  5. Flow =9 kHz or 100 KHz (Depending upon the installed option)

When the frequency settings satisfy the conditions shown above, the Set Freq Low Pass key is displayed in gray.

Setting display range

The E5071C has the following limitations on the display range you can set.

Tspan is the measurement range expressed in time obtained in Measurement range.

The number of response points displayed on the graph is the same as the number of points regardless of the response resolution.

Operation

  1. Press Channel Next/Channel Prev keys and Trace Next/Trace Prev to activate the trace for which you want to set the display range.

  2. Press Analysis key, then click Transform to display the "Transform" menu.

  3. Press each of the following softkeys and then specify the display range. Distance corresponding to the setting time is displayed at the side of the set value in the data entry bar. The displayed distance is a value taking the velocity factor into consideration.
     

    Softkey

    Function

    Start

    Sets the start value of the display range in time

    Stop

    Sets the stop value of the display range in time

    Center

    Sets the center value of the display range in time

    Span

    Sets the span of the display range in time

  4. You cannot use hardkeys to set the display. The hardkeys are dedicated to specifying the sweep range.

Enabling transformation function

Operation

  1. Press Channel Next/Channel Prev keys and Trace Next/Trace Prev to  activate the trace for which you want to use the transformation type.

  2. Press Analysis key, then click Transform to display the "Transform" menu.

  3. Press Transform to enable (ON) the transformation function.

  4. The following requirements must be met to enable the transformation function.