A warning message is displayed in the instrument message/Warning area in the lower left part of the display against a gray background. Pushing a front panel key or executing :DISP:CCL command clears the message.
This message simply appears on the display, being not known to a remote environment such as a GPIB. This message is not displayed when another error (against a red background) has already been displayed in the instrument message/Warning area.
|
Messages |
Description |
|
Arbitrary Segment is not compatible with Swept Seep Mode |
Sweep type should be Stepped when you turn the arbitrary segment on. |
|
Auto port extension not allowed |
This message appears when you try to execute the auto port extension when the sweep type is power sweep or the frequency offset function is ON. If this message is displayed, the auto port extension is not available. |
|
Calibration extrapolated |
The frequency range that can be calibrated with the ECal module is exceeded. In this case, the calibration data for the minimum frequency or maximum frequency are used instead of the data exceeding the allowable frequency range for calibration. |
|
Failed to set zero type of power meter |
This error occurs when zero type (External or Internal) of power meter cannot be performed. |
|
Failed to zero and calibrate power meter |
This error occurs when zeroing or calibration of power meter cannot be performed. |
|
Fixture simulator not allowed |
This message appears when enabling the frequency offset, while the fixture simulator function is turned on. If this message is displayed, the fixture simulator function is automatically turned off. |
|
Log sweep requires 2 octave minimum span |
If you change the sweep range that does not satisfy the necessary condition of the frequency span (the stop frequency is about 4 times or more of the start frequency) when the sweep type is set to the log sweep, this message is displayed. If this message is displayed, the sweep type is automatically set to the linear sweep. For example, if you attempt to change the log type to the log sweep when the start frequency is set to 1 MHz and the stop frequency to 2 MHz, this error occurs. Set the stop frequency to a value of about 4 times or more the start frequency and then set the low seep. |
|
Peak not found |
This warning message is displayed when, with the tracking turned on, the peak specified by the marker search has not been found by the time the sweep is finished (with the tracking executed). |
|
Segment table changed |
This warning message is displayed when the setting specified segment by segment in the segment table is automatically changed by a change in the other setting. For example, this warning message is displayed when, with the power specified segment by segment in the segment table, the power setting for a segment is adjusted by a change in the power range setting. |
|
Sweep mode changed to stepped sweep |
This message appears when you set the sweep type to power sweep, power slope function to enabled (ON, correction coefficient is other than zero), power calibration to ON, frequency offset to enabled, spurious avoidance of frequency offset to enabled, or external signal source control to enabled, while the sweep mode is set to swept mode. When this message is displayed, the sweep mode is automatically set to step mode (during swept mode). |
|
Target value not found |
This warning message is displayed when, with the tracking turned on, the target specified by the marker search has not been found by the time the sweep is finished (with the tracking executed). This warning message is displayed also when, with the bandwidth marker displayed, the setting for the bandwidth marker is changed at the end of the sweep, or when, with the active marker changed or moved, the bandwidth is not found. |
|
Transform, Gate not allowed |
This message appears when you have set the measurement points to two, sweep type to other than linear sweep, or frequency offset to enabled, while the gating/conversion function of the time domain feature is turned on. If this message is displayed, the gating/conversion function is automatically turned off. |
|
User Preset File not found |
This warning message is displayed if no user preset file (D:\UserPreset.sta) exists when executing the SYST:UPR command. |