Other topics about Setting Control Functions
The preset function can be executed without displaying the OK and Cancel softkey buttons when pressing the preset button of the E5071C.
Press System key.
Click Misc Setup > Preset Setup.
Confirm to toggle on (show)/off (hide) the confirmation buttons.
You can save the instrument state of the E5071C into a file in the mass storage, and then recall it with the preset function to reproduce that state.
If no user preset instrument state is stored, you cannot set the user preset function.
Press System key.
Click Misc Setup > Preset Setup > State.
Use one of the following keys for the desired setting.
|
Softkey |
Function |
|
Factory |
Specifies the normal preset function. |
|
User |
Specifies the user-preset function. |
|
Cancel |
Returns to the softkey display in one upper level. |
To execute the user-preset function, you must have a preset setting file that has been saved. Follow these steps to save a preset instrument state of the E5071C.
Press Save/Recall key.
Press Save State > User Pres.