Other topics about Maintenance
This section provides information on how to mount and remove a removable hard disk as well as write the system correction data.
For calibration or repair of the E5071C, send it with the removable hard disk mounted.
If you replace the removable hard disk, make sure to retrieve the system correction data and option data after mounting the hard disk
Back up the license key file for software option before removing hard disk.
Place the license key file after mounting the hard disk.
Follow the steps below to remove a removable hard disk.
Turn off the power.
Insert the key (furnished, Keysight Part Number 0960-2562) in the lock and turn clockwise.
Press the button under the lock and remove the hard disk. It may be too rigid to remove by fingers. In that case, use some tool such as a flat-blade screw driver to remove it.

Do not attempt to unlock the key and remove the hard disk when the power is on. Doing so will turn off the power automatically.
Be careful not to be hurt your hands while removing the hard disk.
Follow the steps below to mount a removable hard disk.
Insert the hard disk into the slot.
Turn the key to the left until it is locked.
Remove the key.
Turn on the E5071C.
The "U" is displayed at the 8 segment LED on next to the removal hard disk when E5071C is turned on without key lock.
The key is available to remove even in Unlocked state. Before power on, confirm if Removable hard disk is locked completely.
Follow the steps below to remove a removable hard disk.
Turn off the power.
Insert the key (furnished, Keysight Part Number 5188-4426) in the lock and turn anti-clockwise.

Open the screw in clockwise direction.

Press the button under the screw.

Remove the hard disk.

Do not attempt to unlock the key and remove the hard disk when the power is on. Doing so will turn off the power automatically.
Follow the steps below to mount a removable hard disk.
Insert the hard disk into the slot.
Turn the screw in anti-clockwise direction until it is locked.
Turn the key to the right until it is locked.
Remove the key.
Turn on the E5071C.
The key is available to remove even in Unlocked state. Before power on, confirm if Removable hard disk is locked completely.
The following procedure shows how to write the system correction data stored in the backup memory to the newly mounted removable hard disk.
Turn on the E5071C.
Press Macro Setup key.
Click Load Project... in the softkey menu.
Select RestoreSysCorFile.vba from the D:\Agilent\Service folder and then press the Open button.
Press Macro Run key
The RestoreSysCorFile dialog box appears.
Click OK.
Once the program has terminated, restart the E5071C to enable the system correction data.