Solid State Drive (SSD) Optimization

Other topics about Maintenance

Overview

The E5071C with HDD revision CHxxxx has a Solid State Drive (SSD) as a storage. The SSD Optimization allows you to keep the best performance for the Solid State Drive.

The SSD Optimization is executed at the following time at the factory setting.

The execution is very quick. Users may not even notice this execution.

Scheduling SSD Optimization

When you want to change the schedule of the SSD Optimization execution, follow the procedure below.

  1. From Windows Start, click Control Panel > Scheduled Tasks  so that Scheduled Tasks in the file explore is displayed.

  2. Double-Click SSD_TRIM.

  3. Select Schedule tab.

  4. Change the schedule you desired.