This section provides useful information to migrate the automation system from 8753 to ENA.
Other topics about Replacing 8753ES with E5071C
The code conversion assistant editor helps to convert 8753 GPIB commands to ENA commands. This software consists of a text editor (EmEditor) and a plug-in software, which works on a PC and helps to edit programs in text format. The editor is also useful for 872X analyzers as most of the 872X commands are the same as 8753’s. The software can be downloaded from www.keysight.com/find/ena_support.
The ENA8753cXL is a code emulation application that allows you to use the ENA with the test program that was written in language for 8753 series network analyzer. This application works on background of the ENA, translating incoming 8753 commands via GPIB in real time.
The ENA8753cXL is designed to work with certain legacy Keysight Network Analyzer products. Not all products may be supported nor can all legacy commands be supported. ALWAYS REFER TO THE INFORMATION PROVIDED IN THE HELP FILE FOR ADDITIONAL INFORMATION REGARDING THE LIST OF SUPPORTED COMMANDS AND PRODUCTS.
On the HDD revision CN920 or above, the installer is pre-loaded on the ENA HDD image (D:\Agilent\ENACXL\Keysight_ENA8753CXL.msi). To install the ENA8753cXL application, follow the instruction below.
If the HDD revision is less than CN920, contact your nearest Keysight Technologies sales representative.
1. Terminate the ENA application: Press System key, click Service > Exit
2. Double-click the Keysight_ENA8753CXL.msi to launch the installer
3. Follow the wizard to install the ENA8753cXL
After the installation is complete, the following files will be available from the Windows start menu. Refer to the “Help Manual” for more details on launching and using the ENA8753cXL.