|
Measurement |
|
|
8753ES |
E5071C |
|
Reset |
|
|
Can be executed by using the front panel and the GPIB command. |
Can be executed by using the front panel, the GPIB command, and telnet. |
|
Channel |
Number of channels |
|
4 channels |
Up to 36 independent measurement channels. |
|
|
Coupling between channels |
|
Channels 3 and 4 are auxiliary channels for channels 1 and 2 and subject to the same sweep conditions, etc. applicable to channels 1 and 2. |
Channels are independent of each other. |
|
Trace |
|
|
A trace for each channel |
Up to 16 traces. |
|
Measurement parameter |
|
|
|
|
|
S-parameter conversion |
|
|
|
Same |
|
Display format (Data format) |
|
|
|
|
|
Test port output |
Number of ports |
|
|
|
|
|
Frequency |
|
|
The following frequency range is available depending on the option.
|
|
|
Power level |
|
|
|
|
|
Characteristic Impedance |
|
|
|
|
|
Coupled/Uncoupled power levels |
|
You can define Couple/Uncouple between channels and between ports. |
Traces are coupled on the same channel, not between channels. |
|
|
Power slope function |
|
Available |
Available |
|
|
Turning the output On/Off |
|
Allowed |
Available |
|
|
Power range |
Items to be set up |
Per port and per channel. |
No Power Range (one range for entire power level.)
|
|
|
|
Automatic setting |
On/Off setting capability. |
|
|
|
|
Setting range |
Range setting with 10 dBm resolution is definable from between -15 and +10 dBm down to between -85 and -60 dBm. |
|
|
Sweep conditions |
Number of points |
|
3, 11, 21, 26, 51, 101, 201, 401, 801, 1601 |
Arbitrary value from 2 to 1601. (Can be set only when the Channel/trace is set to 1 ch/ 4 Tr 20001 points.) |
|
|
Sweep type |
|
|
|
|
|
List frequency sweep |
Number of list tables |
One for channels 1 and 3 and one for channels 2 and 4, two in total |
One for each channel (16 in total) |
|
|
|
Number of segments per table |
Up to 30 |
Up to 201 |
|
|
|
Creation of a table using GPIB(SCPI) command |
Creating a table using more than one command |
Creating a table using a single command |
|
|
|
Number of points |
1 to 1601 points per segment. |
2 to 200001 points per segment. |
|
|
|
Stepped/swept mode |
stepped mode and swept mode. |
stepped mode and swept mode. Selectable also when list frequency sweep is not performed. |
|
|
|
Sweep of designated segments. |
Allowed |
Not allowed (Always sweeps all segments.) |
|
|
Sweep time |
|
Automatic, Manual (definable from the shortest time to 24 hours) |
Automatic, Manual (range of definable sweep depends on sweep condition) |
|
|
IF bandwidth |
|
10 Hz, 30 Hz, 100 Hz, 300 Hz, |
10 Hz, 15 Hz, 20 Hz, 30 Hz, |
|
|
Averaging |
|
Can be set from 1 to 999. |
Can be set from 1 to 999. |
|
Smoothing |
|
|
The smoothing aperture can be set from 0.05% to 20%. |
Same |
|
Electrical delay |
Transmission line |
|
Compatible with coaxial cables and waveguides |
Same |
|
|
Value |
|
Any value from 0 to 10 seconds |
Any value from -10 to +10 seconds |
|
Phase offset |
|
|
Any value from -360 degree to +360 degree. |
Same |
|
Setting sweep conditions for Couple/Uncouple |
|
|
Channels 1 and 3 and channels 2 and 4 are always coupled. Channels 1 and 2 can be set either at Couple or Uncouple. |
Traces in the same channel are coupled; traces in different channels are not coupled. |
|
Trigger mode |
|
|
|
|
|
Trigger source |
|
|
|
|
|
External trigger line |
|
|
Can be set to High or Low |
Same |