Method (Write-only)
WaitOnSRQ Status, Timeout
Suspends the program for specified time until the RQS/MSS bit (bit 6) of the status byte register changes to 1. (No read)
|
Parameter |
Status |
|
Description |
State of the RQS/MSS bit (read only) |
|
Data type |
Boolean type (Boolean) |
|
Range |
One of the following is returned.
1 has been received within the specified time.
1 has not been received within the specified time due to timeout or abort. |
|
Parameter |
Timeout |
|
Description |
Timeout time |
|
Data type |
Long integer type (Long) |
|
Range |
0 to 2,147,483,647 |
|
Preset value |
-1 (infinity) |
|
Unit |
ms (millisecond) |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Stat As Boolean
SCPI.IEEE4882.CLS
SCPI.STATus.OPERation.PTRansition = 0
SCPI.STATus.OPERation.NTRansition = 16
SCPI.STATus.OPERation.ENABle = 16
SCPI.IEEE4882.SRE = 128
SCPI.TRIGger.SEQuence.SOURce = "bus"
SCPI.INITiate(1).CONTinuous = True
SCPI.TRIGger.SEQuence.IMMediate
WaitOnSRQ Stat, 10000
If Stat = True Then
MsgBox "Done"
End If
No equivalent key is available on the front panel.