Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.EQUation.TEXT = Data
Data = SCPI.CALCulate(Ch).SELected.EQUation.TEXT
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).EQUation.TEXT = Data
Data = SCPI.CALCulate(Ch).TRACe(Tr).EQUation.TEXT
This command sets/gets the equation in the Equation Editor. For valid parameters that can be used in this equation, refer to the Equation Editor.
In revision A.9.60 and above, you can select the trace and set/get the equation in the Equation Editor for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Ch |
|
Description |
Channel Number |
|
Range |
1 to 36 |
|
Parameter |
Data |
|
Description |
Sets/Gets the equation in the Equation Editor |
|
Data type |
Character string type (String) |
Dim strEq As String
SCPI.CALCulate(1).SELected.EQUation.TEXT = “Example=S21/(1-S11)”
strEq = SCPI.CALCulate(1).SELected.EQUation.TEXT
SCPI.CALCulate(Ch).SELected.EQUation.STATE
SCPI.CALCulate(Ch).SELected.EQUation.VALid
No equivalent key is available on the front panel for Equation Text but Equation Editor can be accessed through Display > Equation Editor.
All revision:
:CALCulate{[1]-160}[:SELected]:EQUation:TEXT <string1>
:CALCulate{[1]-160}[:SELected]:EQUation:TEXT?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:EQUation:TEXT <string1>
:CALCulate{[1]-160}:TRACe{[1]-16}:EQUation:TEXT?
<string 1><^END>
10 OUTPUT 717;":CALC1:SELected:EQUation:TEXT?"
30 ENTER 717;A$