SCPI.CALCulate(Ch).TRACe(Tr).HOLD.CLEar

Object type

Method (Write-only)

Syntax

SCPI.CALCulate(Ch).TRACe(Tr).HOLD.CLEar

Description

This command clears/resets the trace hold function that holds the active trace at either the maximum or minimum point. This command is supported in revision A.11.20 and above.

Examples

SCPI.CALCulate(1).TRACe(1).HOLD.CLEar

Related objects

SCPI.CALCulate(Ch).TRACe(Tr).HOLD.TYPE

Equivalent key

Display > Data Hold>Restart

Equivalent SCPI command

Syntax

:CALCulate{[1]-160}:TRACe{[1]-16}:HOLD:CLEar

Example of use

10 OUTPUT 717;":CALC1:TRAC1:HOLD:CLE"