Property (Read-Write)
SCPI.CALCulate(Ch).TRACe(Tr).HOLD.TYPE = Status
Status = SCPI.CALCulate(Ch).TRACe(Tr).HOLD.TYPE
This command sets/gets maximum/minimum trace hold function to hold the active trace at the maximum or minimum point. This command is supported in revision A.11.20 and above.
|
Parameter |
Status |
|
Description |
Hold the active trace at the maximum or minimum point. |
|
Data type |
Character string type (String) |
|
Range |
Select from the following:
|
|
Preset value |
"OFF" |
Dim THold As String
SCPI.CALCulate(1).TRACe(1).HOLD.TYPE = "MAXimum"
THold = SCPI.CALCulate(1).TRACe(1).HOLD.TYPE
SCPI.CALCulate(Ch).TRACe(Tr).HOLD.CLEar
Display > Data Hold > OFF|Minimum|Maximum
:CALCulate{[1]-160}:TRACe{[1]-16}:HOLD[:TYPE] {OFF|MIN|MAX}
:CALCulate{[1]-160}:TRACe{[1]-16}:HOLD[:TYPE]?
{OFF|MIN|MAX}<newline><^END>
10 OUTPUT 717;":CALC1:TRAC1:HOLD MIN"
20 OUTPUT 717;":CALC1:TRAC1:HOLD?"
30 ENTER 717;A$