Property (Read-Write)
SCPI.CALCulate(Ch).FSIMulator.BALun.TOPology.BBALanced.PPORts = Ports
Ports = SCPI.CALCulate(Ch).FSIMulator.BALun.TOPology.BBALanced.PPORts
This command assigns each port when the balance device type is "balance-balance", for the selected channel (Ch).
To set the balance device type to "balance-balance," specify BBAL with the SCPI.CALCulate(Ch).FSIMulator.BALun.DEVice object.
Parameter |
Ports |
Description |
Indicates 4-element array data (port number).
The index of the array starts from 0. |
Data type |
Variant type (Variant) |
Range |
1 to 4 |
Preset value |
Ports(0):1 / Ports(1):2 / Ports(2):3 / Ports(3):4 |
Resolution |
1 |
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. If you specify the same port number to 2 or more port numbers, an error occurs when executed. |
Dim BbalPort As Variant
SCPI.CALCulate(1).FSIMulator.BALun.DEVice = "bbal"
SCPI.CALCulate(1).FSIMulator.BALun.TOPology.BBALanced.PPORts = Array(3,4,1,2)
BbalPort = SCPI.CALCulate(1).FSIMulator.BALun.TOPology.BBALanced.PPORts
Dim BbalPort(3) As Variant
Dim Ref As Variant
BbalPort(0) = 3
BbalPort(1) = 4
BbalPort(2) = 1
BbalPort(3) = 2
SCPI.CALCulate(1).FSIMulator.BALun.DEVice = "bbal"
SCPI.CALCulate(1).FSIMulator.BALun.TOPology.BBALanced.PPORts = BbalPort
Ref = SCPI.CALCulate(1).FSIMulator.BALun.TOPology.BBALanced.PPORts
SCPI.CALCulate(Ch).FSIMulator.BALun.DEVice
Analysis > Fixture Simulator > Topology > Port1(bal)
Analysis > Fixture Simulator > Topology > Port2(bal)
When performing the operation from the front panel, set each port separately.
:CALCulate{[1]-160}:FSIMulator:BALun:TOPology:BBALanced
[:PPORts] <numeric 1>, <numeric 2>,<numeric 3>,<numeric 4>
:CALCulate{[1]-160}:FSIMulator:BALun:TOPology:BBALanced
[:PPORts]?
{numeric 1},{numeric 2},{numeric 3},{numeric 4}<newline><^END>
10 OUTPUT 717;":CALC1:FSIM:BAL:TOP:BBAL 1,2,3,4"
20 OUTPUT 717;":CALC1:FSIM:BAL:TOP:BBAL?"
30 ENTER 717;A,B,C,D