Property (Read Only)
All revision:
Data = SCPI.CALCulate(Ch).SELected.FUNCtion.DATA
In revision A.9.60 and above, the following syntax is also supported:
Data = SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.DATA
This command reads the analysis result of the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object, for the active trace of selected channel (Ch).
In revision A.9.60 and above, you can select the trace and read the analysis result of the SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute object for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Data |
|
Description |
Indicates the array data (analysis result) of N (number of data pairs)x2. N (number of data pairs) can be read out with the SCPI.CALCulate(Ch).SELected.FUNCtion.POINts object. Where n is an integer between 1 and N.
The index of the array starts from 0. |
|
Data type |
Variant type (Variant) |
Dim AnaData As Variant
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.FUNCtion.TYPE = "mean"
SCPI.CALCulate(1).SELected.FUNCtion.EXECute
AnaData = SCPI.CALCulate(1).SELected.FUNCtion.DATA
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.FUNCtion.TYPE
SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute
SCPI.CALCulate(Ch).SELected.FUNCtion.POINts
No equivalent key is available on the front panel.
All revision:
:CALCulate{[1]-160}[:SELected]:FUNCtion:DATA?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCtion:DATA?
<numeric 1>,… ,<numeric N*2><^END>
10 OUTPUT 717;":CALC1:FUNC:POIN?"
20 ENTER 717;A
30 REDIM B(1:2*A)
40 OUTPUT 717;":CALC1:FUNC:DATA?"
50 ENTER 717;B(*)