Property (Read Only)
All revision:
Status = SCPI.CALCulate(Ch).SELected.LIMit.FAIL
In revision A.9.60 and above, the following syntax is also supported:
Status = SCPI.CALCulate(Ch).TRACe(Tr).LIMit.FAIL
This command reads the limit test result, for the active trace of selected channel (Ch).
In revision A.9.60 and above, you can select the trace and read the limit test result for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Status |
|
Description |
Limit test result |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following:
|
|
Note |
When the limit test is set to OFF, False or OFF is always read out. |
Dim Result As Boolean
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.LIMit.STATe = True
Result = SCPI.CALCulate(1).SELected.LIMit.FAIL
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.LIMit.STATe
No equivalent key is available on the front panel.
All revision:
:CALCulate{[1]-160}[:SELected]:LIMit:FAIL?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:LIMit:FAIL?
{1|0}<newline><^END>
|
|
Description |
|
1 |
The limit test result is FAIL. |
|
0 |
The limit test result is PASS. |
When the limit test is set to OFF, 0 is always read out.
10 OUTPUT 717;":CALC1:LIM:FAIL?"
20 ENTER 717;A