Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.LIMit.OFFSet.STIMulus = Value
Value = SCPI.CALCulate(Ch).SELected.LIMit.OFFSet.STIMulus
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).LIMit.OFFSet.STIMulus = Value
Value = SCPI.CALCulate(Ch).TRACe(Tr).LIMit.OFFSet.STIMulus
This command sets/gets the stimulus offset of the limit line, for the selected channel (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command).
The setting of the limit line doesn't change even if the offset value is changed.
In revision A.9.60 and above, you can select the trace and set/get the stimulus offset of the limit line for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Value |
|
Description |
The stimulus offset of the limit line |
|
Data type |
Double precision floating point type (Double) |
|
Range |
-1E12 to 1E12 |
|
Preset value |
0 |
|
Unit |
Hz (hertz), dBm or second |
For information on the variable (Ch), see Variable.
Dim LimOffset As Double
SCPI.CALCulate(1).SELected.LIMit.OFFSet.STIMulus = 1E9
LimOffset = SCPI.CALCulate(1).SELected.LIMit.OFFSet.STIMulus
SCPI.CALCulate(Ch).SELected.LIMit.STATe
SCPI.CALCulate(Ch).SELected.LIMit.OFFSet.AMPLitude
SCPI.CALCulate(Ch).SELected.LIMit.OFFSet.MARKer
Analysis > Limit Test > Limit Line Offsets > Stimulus Offset
All revision:
:CALCulate{[1]-160}[:SELected]:LIMit:OFFSet:STIMulus <numeric>
:CALCulate{[1]-160}[:SELected]:LIMit:OFFSet:STIMulus?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:LIMit:OFFSet:STIMulus <numeric>
:CALCulate{[1]-160}:TRACe{[1]-16}:LIMit:OFFSet:STIMulus?
{numeric}<newline><^END>
10 OUTPUT 717;":CALC1:LIM:OFFS:STIM 5E3"
20 OUTPUT 717;":CALC1:LIM:OFFS:STIM?"
30 ENTER 717;A