Property (Read Only)
All revision:
Value = SCPI.CALCulate(Ch).SELected.LIMit.REPort.POINts
In revision A.9.60 and above, the following syntax is also supported:
Value = SCPI.CALCulate(Ch).TRACe(Tr).LIMit.REPort.POINts
This command reads the number of the measurement points that failed the limit test, for the active trace of selected channel (Ch).
In revision A.9.60 and above, you can select the trace and read the number of the measurement points that failed the limit test, for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Value |
|
Description |
Number of measurement points that failed |
|
Data type |
Long integer type (Long) |
|
Preset Value |
0 |
Dim FailPoin As Long
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.LIMit.STATe = True
FailPoin = SCPI.CALCulate(1).SELected.LIMit.REPort.POINts
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.LIMit.STATe
No equivalent key is available on the front panel.
All revision:
:CALCulate{[1]-160}[:SELected]:LIMit:REPort:POINts?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:LIMit:REPort:POINts?
{numeric}<newline><^END>
10 OUTPUT 717;":CALC1:LIM:REP:POIN?"
20 ENTER 717;A