Method (Write-only)
All revision:
SCPI.CALCulate(Ch).SELected.MARKer(Mk).FUNCtion.EXECute
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).MARKer(Mk).FUNCtion.EXECute
This command executes search with marker 1 to 9 (Mk) and reference marker (Mk:10), for the active trace of selected channel (Ch).
To specify the type of the search, use the SCPI.CALCulate(Ch).SELected.MARKer(Mk).FUNCtion. TYPE object. (No read)
In revision A.9.60 and above, you can select the trace and execute search with marker 1 to 9 (Mk) and reference marker (Mk:10), for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.MARKer(1).FUNCtion.TYPE = "maximum"
SCPI.CALCulate(1).SELected.MARKer(1).FUNCtion.EXECute
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.MARKer(Mk).FUNCtion.TYPE
SCPI.CALCulate(Ch).SELected.MARKer.FUNCtion.DOMain.STATe
Marker Search > Max|Min
Marker Search > Peak > Search Peak|Search Left|Search Right
Marker Search > Target > Search Target|Search Left|Search Right
When performing the operation from the front panel, you select the search type and execute the search at the same time.
All revision:
:CALCulate{[1]-160}[:SELected]:MARKer{[1]-10}:FUNCtion:EXECute
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:MARKer{[1]-10}:FUNCtion:EXECute
10 OUTPUT 717;":CALC1:MARK1:FUNC:EXEC"