SCPI.CALCulate(Ch).SELected.MATH.MEMorize

Object type

Method (Write-only)

Syntax

All revision:

SCPI.CALCulate(Ch).SELected.MATH.MEMorize

 

In revision A.9.60 and above, the following syntax is also supported:

SCPI.CALCulate(Ch).TRACe(Tr).MATH.MEMorize

Description

This command copies the measurement data to the memory trace, for the active trace of selected channel (Ch).

 

In revision A.9.60 and above, you can select the trace and copy the measurement data to the memory trace, for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.

Examples

SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.MATH.MEMorize

Related objects

SCPI.CALCulate(Ch).PARameter(Tr).SELect

Equivalent key

Display > Data -  > Mem

Equivalent SCPI command

Syntax

All revision:

:CALCulate{[1]-160}[:SELected]:MATH:MEMorize

 

 In revision A.9.60 and above, the following syntax is also supported:

:CALCulate{[1]-160}:TRACe{[1]-16}:MATH:MEMorize

Example of use

10 OUTPUT 717;":CALC1:MATH:MEM"