Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.MIXer.XAXis = Param
Param = SCPI.CALCulate(Ch).SELected.MIXer.XAXis
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).MIXer.XAXis = Param
Param = SCPI.CALCulate(Ch).TRACe(Tr).MIXer.XAXis
This command sets/gets the X-axis frequency when the frequency offset feature is off, for the active trace of selected channel (Ch).
In revision A.9.60 and above, you can select the trace and set/get the X-axis frequency when the frequency offset feature is off for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Param |
|
Description |
Selects the X-axis frequency (frequency offset: off) |
|
Data type |
Character string type (String) |
|
Range |
Select from the following:
|
|
Preset value |
"NORMal" |
Dim Xaxis As String
SCPI.SENSe.OFFSet.STATe = False
SCPI.CALCulate(1).SELected.MIXer.XAXis = "RFPLo"
Xaxis = SCPI.CALCulate(1).SELected.MIXer.XAXis
SCPI.CALCulate(Ch).SELected.OFFset.XAXis
Sweep Setup > Frequency Offset > X-Axis > Normal|RF+LO|RF-LO|LO-RF
All revision:
:CALCulate{[1]-160}[:SELected]:MIXer:XAXis {NORMal|RFPLo| RFMLo|LOMRf}
:CALCulate{[1]-160}[:SELected]:MIXer:XAXis?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:MIXer:XAXis {NORMal|RFPLo| RFMLo|LOMRf}
:CALCulate{[1]-160}:TRACe{[1]-16}:MIXer:XAXis?
{NORM|RFPL|RFML|LOMR}<newline><^END>
10 OUTPUT 717;":CALC1:MIX:XAX RFPL"
20 OUTPUT 717;":CALC1:MIX:XAX?"
30 ENTER 717;A$