Property (Read-Write)
All revision:
SCPI.CALCulate(Ch).SELected.SMOothing.STATe = Status
Status = SCPI.CALCulate(Ch).SELected.SMOothing.STATe
In revision A.9.60 and above, the following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).SMOothing.STATe = Status
Status = SCPI.CALCulate(Ch).TRACe(Tr).SMOothing.STATe
This command turns ON/OFF the smoothing, for the active trace of selected channel (Ch).
In revision A.9.60 and above, you can select the trace and turn ON/OFF the smoothing for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Status |
|
Description |
ON/OFF of the smoothing |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following:
|
|
Preset value |
False or 0 |
Dim Smo As Boolean
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.SMOothing.STATe = True
Smo = SCPI.CALCulate(1).SELected.SMOothing.STATe
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.SMOothing.APERture
Avg > Smoothing
All revision:
:CALCulate{[1]-160}[:SELected]:SMOothing[:STATe] {ON|OFF|1|0}
:CALCulate{[1]-160}[:SELected]:SMOothing[:STATe]?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:SMOothing[:STATe] {ON|OFF|1|0}
:CALCulate{[1]-160}:TRACe{[1]-16}:SMOothing[:STATe]?
{1|0}<newline><^END>
10 OUTPUT 717;":CALC1:SMO:STAT ON"
20 OUTPUT 717;":CALC1:SMO:STAT?"
30 ENTER 717;A