Property (Read-Write)
SCPI.FORMat.DATA = Param
Param = SCPI.FORMat.DATA
This command can be used to set/get format data using the following SCPI commands:
:CALC{1-160}:DATA:FDAT
:CALC{1-160}:DATA:FMEM
:CALC{1-160}:DATA:SDAT?
:CALC{1-160}:DATA:SMEM?
:CALC{1-160}:FUNC:DATA?
:CALC{1-160}:LIM:DATA
:CALC{1-160}:LIM:REP?
:CALC{1-160}:LIM:REP:ALL?
:CALC{1-160}:BLIM:REP?
:CALC{1-160}:RLIM:DATA?
:CALC{1-160}:RLIM:REP?
:SENS{1-160}:CORR:COEF
:SENS{1-160}:FREQ:DATA?
:SENS{1-160}:SEGM:DATA
:SOUR:POW:PORT:CORR:COLL:TABL:ASEN:DATA
:SOUR:POW:PORT:CORR:COLL:TABL:BSEN:DATA
:SOUR{1-160}:POW:PORT{1-4}:CORR:COLL:TABL:LOSS:DATA
:SOUR{1-160}:POW:PORT{1-4}:CORR:DATA
ASCII transfer format must be specified when controlling the E5071C using SCPI commands with the Parse object in the E5071C VBA.
Selection of the data format determines the result format of SCPI.CALCulate(Ch).SELected.DATA.XAXis.
|
Parameter |
Param |
|
Description |
Data transfer format |
|
Data type |
Character string type (String) |
|
Range |
Select from the following: "ASCii": Specifies the ASCII transfer format. "REAL": Specifies the IEEE 64-bit floating point binary transfer format. "REAL32": Specifies the IEEE 32-bit floating point binary transfer format. |
|
Preset value |
"ASCii" |
Dim Fmt As String
SCPI.FORMat.DATA = "ASC"
Fmt = SCPI.FORMat.DATA
SCPI.CALCulate(Ch).SELected.DATA.XAXis
No equivalent key is available on the front panel.
:FORMat:DATA {ASCii|REAL|REAL32}
:FORMat:DATA?
{ASC|REAL|REAL32}<newline><^END>
10 OUTPUT 717;":FORM:DATA REAL"
20 OUTPUT 717;":FORM:DATA?"
30 ENTER 717;A$