Property (Read Only)
All revision:
Data = SCPI.CALCulate(Ch).SELected.DATA.XAXis
In revision A.9.60 and above, the following syntax is also supported:
Data = SCPI.CALCulate(Ch).TRACe(Tr).DATA.XAXis
This command reads the data of measurement points of X axis, for the active trace of selected channel (Ch).
In revision A.9.60 and above, you can select the trace and read the data of measurement points of X axis for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Data |
|
Description |
Indicates the array data (measurement points) of X axis |
|
Data type |
Variant type (Variant) |
Dim AnaData As Variant
AnaData = SCPI.CALC1.SEL.DATA.XAX
No equivalent key is available on the front panel.
All revision:
:CALCulate{[1]-160}[:SELected]:DATA:XAXis?
In revision A.9.60 and above, the following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:DATA:XAXis?
<numeric 1>,… ,<numeric N><^END>
10 OUTPUT 717;":CALC1:SEL:DATA:XAX?"
20 ENTER 717;A(*)