Method (Write-only)
Value = SCPI.HCOPy.IMMediate
This command outputs the display image on the LCD display to the printer connected to the E5071C.
When printing the E5071C measurement screen, execute the VBA program with the Visual Basic editor closed. For the method, see Running a Program from the E5071C Measurement Screen.
SCPI.HCOPy.IMMediate
[System] > Print
When performing the operation from the front panel, the image on the LCD display memorized in the volatile memory (clipboard) (the image on the LCD display when the [Capture] ([System]) key is pressed) is printed. If no image is memorized in the clipboard, in the same way as the SCPI.HCOPy.IMMediate object, the image on the LCD display at the execution is memorized in the clipboard and then it is printed.
:HCOPy[:IMMediate]
10 OUTPUT 717;":HCOP"